PORT_DEVICE not defined

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PORT_DEVICE not defined

1,403 Views
jonbuckman
Contributor I

Why do I get this error;  'PTC_PORT_DEVICE' undeclared (first use in this function) even though I have PTC:Init_GPIO and PORTC:Init_PORT in components?

Labels (1)
0 Kudos
Reply
1 Reply

1,332 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Jon

I think  "PTC_PORT_DEVICE" maybe a maro definition included in a header file  ,find it and include it.

If this is not working,  you can screenshot about "PTC_PORT_DEVICE"  or send the project to us.

Hope this helps.

Regards,

Alice

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply