PBL RCW

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PBL RCW

3,637 Views
yoshida08
Contributor I

How can I use CodeWarrior to check if the PBL RCW data from the SD card is loaded?
?

0 Kudos
Reply
5 Replies

3,561 Views
yoshida08
Contributor I

We could solve the problem that HRESET does not change to High on our design board.

IFC_AVD signal was problem, signal was Low level. 

0 Kudos
Reply

3,562 Views
yoshida08
Contributor I

Thank you for your reply.

I'm sorry, I reply late.

I will confirm contents of your reply.

0 Kudos
Reply

3,603 Views
Chavira
NXP TechSupport
NXP TechSupport

Hello yoshida08!

You can Read/Write the PBL RCW in the Code Warrior.

Example_1.png

You have to click on PBL1:PBL at the bottom left on the window "'components"' and then in the part of properties in the right you can configure the PBL RCW.

Example_2.png

In the window "'validation"" you can write the new configuration to your device.

And if you prefer import a configuration you can read a device too.

Best regards!

0 Kudos
Reply

3,624 Views
yoshida08
Contributor I

Thank you for your reply.

We are using LS1043A.

We cannot solve the problem that HRESET does not change to High on our design board.

0 Kudos
Reply

3,634 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

Could you tell me what kind of MCU you are using?

Best regards,
Pavel

0 Kudos
Reply