PBL/RCW for T1024

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PBL/RCW for T1024

5,375 Views
gouravjain
Contributor IV

Hello All,

 

I am beginner for freescale processorsand handling first time T1024 processor. Can any body tell me how to open RCW configuration settings on Codewarrior tool?? I'm not able to find how to create QorIQ project in Codewarrior 10.5.1 tool.

 

Help would be highly appreciated..

 

Thanks,

Gourav

Labels (1)
Tags (1)
0 Kudos
Reply
8 Replies

4,687 Views
chenxiaoyong
Contributor I

I downloaded and installed this tool successfully based on above steps, and my CodeWarrior is as following:

Installed Products:

- CodeWarrior for Power Architecture

  Version: 10.5.1

  Build Id:160128

Hope this will help you, I am also debugging this device, some problems as well.

T1024 in hardcoded mode

Hope somebody can help on this problem, thanks.

0 Kudos
Reply

4,687 Views
addiyi
NXP Employee
NXP Employee

You have to install QCVS on top of CW for PA. For this you have to go to Help > Install New Software and select as updatesite: FSL PA QCVS - http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.qcvs_win.

Adrian

0 Kudos
Reply

4,687 Views
gouravjain
Contributor IV

Hi Adrian,

Thanks for your prompt reply.... but its giving below error while followed your instruction..

Forbidden

You don't have permission to access /lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.qcvs_win/ on this server.

gourav

0 Kudos
Reply

4,687 Views
addiyi
NXP Employee
NXP Employee

That link can be use only in Help > Install New Software. So, open CW and go to Help > Install New Software, select the link and the QCVS 4.5 as in below image.

pastedImage_0.png

0 Kudos
Reply

4,687 Views
gouravjain
Contributor IV

Hi Adrian,

After downloading around 40-50 % (not only QCVS tool even plugin also) im getting below error,

An error occurred while collecting items to be installed

session context was:(profile=PlatformProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).

Unable to read repository at http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.qcvs_win/plugins/org.eclipse.....

Read timed out.

Pls help me out from this problem .

Thanks,

Gourav

0 Kudos
Reply

4,687 Views
gouravjain
Contributor IV

And one more question, cant be use Codewarrior 10.3.3v for T1024 processor??

0 Kudos
Reply

4,687 Views
addiyi
NXP Employee
NXP Employee

CodeWarrior for PA 10.3.3 doesn't provide support for T1024. Please use 10.5.1. Also, about the QCVS installation please try again or search on nxp.com/qcvs the offline installation package.

Adrian

0 Kudos
Reply

4,687 Views
gouravjain
Contributor IV

Hi Adrian,

Thanks for your prompt help. Now i followed offline way to install QCVS and it worked in my system.

--

Gourav

0 Kudos
Reply