P3041DS Hydra Problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P3041DS Hydra Problem

2,002 次查看
dmitrshard
Contributor II

Hello!

 

I try to launch helloWorld project through CodeWarrior Tap (Download debug configuration) and have problem. See screenshot. What i need to avoid this error?

Original Attachment has been moved to: dada.zip

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,831 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Dmitr Shard,

There is no argument "CCM/BPTRAR" in the default CW initialization file, and I didn't encounter this problem when initialize the target with the default CW initialization file.

So would you please provide your CW initialization file which you specified from Run->Debug Configurations-><project>-core00_RAM_p3041_Download->Edit->Edit->Initialization->Initialize target script?

And which version CodeWarrior do you use?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,831 次查看
addiyi
NXP Employee
NXP Employee

Did you use bareboard project generated by wizard? Did you select P3041DSHydra as board? Also, please check the init file used.

Adrian

0 项奖励
回复