P3041DS Hydra Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P3041DS Hydra Problem

2,017件の閲覧回数
dmitrshard
Contributor II

Hello!

 

I try to launch helloWorld project through CodeWarrior Tap (Download debug configuration) and have problem. See screenshot. What i need to avoid this error?

Original Attachment has been moved to: dada.zip

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,846件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Dmitr Shard,

There is no argument "CCM/BPTRAR" in the default CW initialization file, and I didn't encounter this problem when initialize the target with the default CW initialization file.

So would you please provide your CW initialization file which you specified from Run->Debug Configurations-><project>-core00_RAM_p3041_Download->Edit->Edit->Initialization->Initialize target script?

And which version CodeWarrior do you use?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,846件の閲覧回数
addiyi
NXP Employee
NXP Employee

Did you use bareboard project generated by wizard? Did you select P3041DSHydra as board? Also, please check the init file used.

Adrian

0 件の賞賛
返信