P3041DS Hydra Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P3041DS Hydra Problem

2,181 Views
dmitrshard
Contributor II

Hello!

 

I try to launch helloWorld project through CodeWarrior Tap (Download debug configuration) and have problem. See screenshot. What i need to avoid this error?

Original Attachment has been moved to: dada.zip

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

2,010 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Dmitr Shard,

There is no argument "CCM/BPTRAR" in the default CW initialization file, and I didn't encounter this problem when initialize the target with the default CW initialization file.

So would you please provide your CW initialization file which you specified from Run->Debug Configurations-><project>-core00_RAM_p3041_Download->Edit->Edit->Initialization->Initialize target script?

And which version CodeWarrior do you use?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,010 Views
addiyi
NXP Employee
NXP Employee

Did you use bareboard project generated by wizard? Did you select P3041DSHydra as board? Also, please check the init file used.

Adrian

0 Kudos
Reply