OVER-RIDING HARDCODED RCW IN LS1043ARDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OVER-RIDING HARDCODED RCW IN LS1043ARDB

ソリューションへジャンプ
2,545件の閲覧回数
nikhilprakash
Contributor IV

Hi,

I am currently working on ls1043ardb board.In our target board there is no provision for sd card booting.How can we over-ride the hardcoded rcw for enabling ifc flash and program it using codewarrior tap  for LS1043ARDB.

Pls help.

 

thanks in advance

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,851件の閲覧回数
addiyi
NXP Employee
NXP Employee

In LS1043 tcc, Target Initialization File provides support for rcw override. You have to set useSafeRCW = True, then Connect to the board.

Adrian

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,852件の閲覧回数
addiyi
NXP Employee
NXP Employee

In LS1043 tcc, Target Initialization File provides support for rcw override. You have to set useSafeRCW = True, then Connect to the board.

Adrian

0 件の賞賛
返信
1,851件の閲覧回数
nikhilprakash
Contributor IV

Thanks Adrian ,it worked

0 件の賞賛
返信