OVER-RIDING HARDCODED RCW IN LS1043ARDB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

OVER-RIDING HARDCODED RCW IN LS1043ARDB

跳至解决方案
2,541 次查看
nikhilprakash
Contributor IV

Hi,

I am currently working on ls1043ardb board.In our target board there is no provision for sd card booting.How can we over-ride the hardcoded rcw for enabling ifc flash and program it using codewarrior tap  for LS1043ARDB.

Pls help.

 

thanks in advance

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,847 次查看
addiyi
NXP Employee
NXP Employee

In LS1043 tcc, Target Initialization File provides support for rcw override. You have to set useSafeRCW = True, then Connect to the board.

Adrian

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,848 次查看
addiyi
NXP Employee
NXP Employee

In LS1043 tcc, Target Initialization File provides support for rcw override. You have to set useSafeRCW = True, then Connect to the board.

Adrian

0 项奖励
回复
1,847 次查看
nikhilprakash
Contributor IV

Thanks Adrian ,it worked

0 项奖励
回复