OVER-RIDING HARDCODED RCW IN LS1043ARDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OVER-RIDING HARDCODED RCW IN LS1043ARDB

Jump to solution
2,630 Views
nikhilprakash
Contributor IV

Hi,

I am currently working on ls1043ardb board.In our target board there is no provision for sd card booting.How can we over-ride the hardcoded rcw for enabling ifc flash and program it using codewarrior tap  for LS1043ARDB.

Pls help.

 

thanks in advance

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,936 Views
addiyi
NXP Employee
NXP Employee

In LS1043 tcc, Target Initialization File provides support for rcw override. You have to set useSafeRCW = True, then Connect to the board.

Adrian

View solution in original post

0 Kudos
Reply
2 Replies
1,937 Views
addiyi
NXP Employee
NXP Employee

In LS1043 tcc, Target Initialization File provides support for rcw override. You have to set useSafeRCW = True, then Connect to the board.

Adrian

0 Kudos
Reply
1,936 Views
nikhilprakash
Contributor IV

Thanks Adrian ,it worked

0 Kudos
Reply