OSBDM for TRK MPC 5604B??

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OSBDM for TRK MPC 5604B??

ソリューションへジャンプ
4,379件の閲覧回数
josealonsovalle
Contributor III

Hi, i am new in the Qorivva microcontroller  and i want to start with the TRK 5604B, but there people saying me that i can not program the micro if i have not a BDM..

 

Is true what i need the BDM for program the micro, i simplify connect the board to the computer with the USB cable directly???

 

this is the device what i need??

 

 

greetings...

ラベル(1)
0 件の賞賛
返信
1 解決策
4,147件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Jose,

I don't have the board on my side but the TRK-MPC5604B: MPC5604B StarterTRAK (Development Kit) should contains all cables to use it.

According to the Quick Start http://cache.freescale.com/files/microcontrollers/doc/user_guide/MPC5604BQSG.pdf, the board includes OSBDM:

      On-board JTAG connection via open source OSBDM circuit using the MPC9S08JM microcontroller

The TRK-MPC5604B package includes the following items:

• TRK-MPC5604B Board

• CodeWarrior Development Studio DVD-ROM

• TRK-MPC5604B Resources CD

• USB A-to-B Cable

• Freescale Warranty Card

The USB A to B cable is using the OSBDM interface.

I will check with my colleague and will keep you updated.

However, following the info I found, it should work.


Have a great day,
Pascal

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,727件の閲覧回数
andy_Musk
Contributor III

the MPC9S08JM microcontroller  need burn firmware or not? if need where is the firmware?

0 件の賞賛
返信
4,147件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Just got info from colleague.

OSBDM/OSJTAG interface works with CW for MCUs v 10.x


You don't need Multilink interface.


Have a great day,
Pascal

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
4,148件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Jose,

I don't have the board on my side but the TRK-MPC5604B: MPC5604B StarterTRAK (Development Kit) should contains all cables to use it.

According to the Quick Start http://cache.freescale.com/files/microcontrollers/doc/user_guide/MPC5604BQSG.pdf, the board includes OSBDM:

      On-board JTAG connection via open source OSBDM circuit using the MPC9S08JM microcontroller

The TRK-MPC5604B package includes the following items:

• TRK-MPC5604B Board

• CodeWarrior Development Studio DVD-ROM

• TRK-MPC5604B Resources CD

• USB A-to-B Cable

• Freescale Warranty Card

The USB A to B cable is using the OSBDM interface.

I will check with my colleague and will keep you updated.

However, following the info I found, it should work.


Have a great day,
Pascal

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信