No boards available in the Project Wizard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No boards available in the Project Wizard

11,211 Views
adrianbica
Contributor II

I am trying to evaluate the Codewarrior 10.5 (never used it before). I installed it on my computer and trying to create a new project with Project Wizard, but when I get to select the board, there is nothing displayed in the window. In the directory C:\Freescale\CW MCU v10.5\MCU\lib\wizard_data I have a lot of xml files, but no board shows up in the Wizard. Am I doing anything wrong? How could I get the boards to appear in Project Wizard?

Please, note that this happens when I try to create a MQX project, it shows board when I select a Bareboard Project

 

Thanks,

Adrian

Labels (1)
0 Kudos
Reply
11 Replies

10,672 Views
Rick_Li
NXP Employee
NXP Employee

Hi Adrian,

Please make sure you have MQX installed in your PC.

and the enclosed document is on how to add a new board supported in CW.

hope it helps!

0 Kudos
Reply

10,672 Views
adrianbica
Contributor II

I do have MQX installed and as I said I already have the folder C:\Freescale\CW MCU v10.5\MCU\lib\wizard_data filled with plenty ox xml files. But they simple don't show in the wizard. Adding another board to that collection, won't help.I can see some boards if I try a MQX Lite project, but not for a MQX 4.0 project

0 Kudos
Reply

10,672 Views
Rick_Li
NXP Employee
NXP Employee

do you means that there is no board list in the new created wizard as showed in the enclosed image?

if so, then, I would suggest re-install your CW and MQX

0 Kudos
Reply

10,672 Views
adrianbica
Contributor II

This is exactly what I mean! There is nothing in that field where you show a list of boards. I did uninstall and reinstall without any improvement.

0 Kudos
Reply

10,672 Views
Rick_Li
NXP Employee
NXP Employee

Hi Adrian,

I'm sorry, the problem still seems a install problem.

could you please try to re-install the latest MQX in the default place (C:\Freescale\Freescale_MQX_4_0).

and then, re-launch the CW.

if the problem still remains, then, I'm afraid you have to re-install your PC.

I'm so sorry!

0 Kudos
Reply

10,672 Views
adrianbica
Contributor II

Could be because I'm running Windows XP?

Adrian Bica

Sr. Software Engineer

Network Technologies Inc.

Phone: (330)-562-7070

Fax: (330)-562-1999

www.networktechinc.com

0 Kudos
Reply

10,672 Views
ARQuattr
Contributor III

Hi Adrian, did you resolve this issue?  I have had a similar problem with MQX4.1.  With 4.0.1 I was able to see the boards in the wizard, but with 4.1, I don't even see "New MQX Project", only "New MQX-Lite Project" is available.

Thanks

0 Kudos
Reply

10,672 Views
Rick_Li
NXP Employee
NXP Employee

the Windows XP is not he root cause.

and I'm also running CW v10.5+MQX 4.0.2 on a Windows XP system.

0 Kudos
Reply

10,672 Views
Rick_Li
NXP Employee
NXP Employee

the latest CW version is 4.0.2

0 Kudos
Reply

10,671 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Freescale MQX only supports several Freescale demo board. not all the Freescale board.

this is documented in MQX4.0 release note: 1.1.3 Target Requirements

see attached.

if user uses other board, he has to port the code to other code by oneself.

Evaluation boards supported:

 Vybrid

o TWR-VF65GS10 Development Kit

 Kinetis

o TWR-K20D50M Development Kit

o TWR-K20D72M Development Kit

o TWR-K21D50M Development Kit

o TWR-K40X256 Development Kit

o TWR-K40D100M Development Kit

o TWR-K53N512 Development Kit

o TWR-K60N512 Development Kit

o TWR-K60D100M Development Kit

o TWR-K60F120M Development Kit

o TWR-K70F120M Development Kit

o KwikStik - K40X256 based Evaluation Board

 ColdFire V1

o TWR-MCF51JF Development Kit

 ColdFire V2

o M52259EVB Evaluation Board

o M52259DEMOKIT Development Kit

o TWR-MCF52259 Development Kit

 ColdFire V4

o TWR-MCF54418 Development Kit

 PowerPC:

o TWR-PXD10 Development Kit

o TWR-PXN20 Development Kit

o TWR-PXS20 Development Kit

o TWR-PXS30 Development Kit

0 Kudos
Reply

10,671 Views
adrianbica
Contributor II

Jennie,

Did you understand my question?

I can see that it supports only several boards (and my board happens to be among them), but I would like to see at least one in the wizard, or, let me somehow to create a new project. I am blocked at this step where is nothing to select!

Adrian

0 Kudos
Reply