No Source available for "' error in codewarrior10 and using ms9s12zvh64 micro

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No Source available for "' error in codewarrior10 and using ms9s12zvh64 micro

2,305 Views
ponalagappan
Contributor III

Hi ,

I am trying to debug my code in codewarrior it is showing following error.

It is showing following error :: No source available for "xx".

I attached screen shot of that error. During build, there is no error.

But while debugging after sometimes it is giving above said error. 

 

In my code i have 2 parts, when one is enabled and other is commented and vice versa

are working. But when i enable both the parts it is giving this problem. There is no dependencies

or shared variable is there between these two parts.

 

How to fix this problem? 

 

 

 

175485_175485.pngISSUE.png"

Labels (1)
0 Kudos
Reply
1 Reply

1,853 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Pon,

Maybe it is caused by a stack-overflow, there also a same question:

URGENT: No source available for "0x000001 (0x000001)() "  

Please check your project as Jens Winkler said .

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply