Need reference documents of codewarrior for certification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need reference documents of codewarrior for certification

Jump to solution
2,563 Views
kiminkim
NXP Employee
NXP Employee


Dear team,

 

Customer needs to get UL1998 which is the certification of their process verifying if their SW development tool is
qualified or not.

 

So they want to have reference documents for qualification of Codewarrior.

They are developing with S08 and Codewarrior IDE 5.9

As their request, below items are
required.

- Revision history

- Bug list

- Review or analysis

- Any suitable documents for qualification.

 

Please share any documents that is helpful to qualification of UL1998.

Thank you

Labels (1)
0 Kudos
Reply
1 Solution
2,396 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Ki

I’m sorry that we have not performed certification of UL1998 qualification for CodeWarrior. We provide customers proven in use documents instead. The attached doc is the proven in use doc for CodeWarrior v6.3.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,397 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Ki

I’m sorry that we have not performed certification of UL1998 qualification for CodeWarrior. We provide customers proven in use documents instead. The attached doc is the proven in use doc for CodeWarrior v6.3.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply