NXP Library Not working with some android devices.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP Library Not working with some android devices.

3,208件の閲覧回数
lakshithagayash
Contributor I

I developed an android application for write and read data to a Mifare desfire ev1 card using nxp-nfc-library-1.7(latest version). That application worked properly with the device which I used for develop the  application (Model - TPS 900, Android version - 7.1.2). But when I try that with another device (Model : TC-TOUCH-T1, Android version - 6.0.0)  It couldn't work properly. It gives an exception "com.nxp.nfclib.exceptions.InvalidResponseLengthExceptionIncomplete" when just selecting the master application(AID-0X000000). Is this because of an android version? Or any other reason?

ラベル(1)
0 件の賞賛
返信
1 返信

3,127件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信