Multilink Universal cannot connect to MCF5566EVB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multilink Universal cannot connect to MCF5566EVB

5,167件の閲覧回数
zwilcox
Contributor IV

I just got an MCF5566EVB eval board.  I'm trying connect with the P&E Multilink Universal that came with it.

I'm using CodeWarrior Development Studio for Freescale MPC55xx and MPC56xx version 2.10, build 120305.

pastedImage_2.png

pastedImage_1.png

When I try to connect, I get the following message in the Status Window:

Debugger retrying force to background mode.  Can not enter background Mode.

In the PEMicro Connection manager, I get a message saying "Can't communicate with the target processor! Please check your connections between the cable and the target and make sure the target has power."

pastedImage_3.png

One thing I've notice, is the PEMICRO Connection Manager is referring to BDM but the MPC5566EVB uses JTAG.

6 返答(返信)

4,376件の閲覧回数
smallyang
Contributor IV

请问你找到安装包了吗,可以发个给我吗  这里的链接都失效了

0 件の賞賛
返信

5,020件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please show me, which version of ICDPPCNEXUS you use in CW 2.10?

I tried with two versions (version 1.34 did not work), but with version 6.83 it works correct.

pastedImage_1.png

Please let me know.

Regards,

Martin

5,020件の閲覧回数
zwilcox
Contributor IV

It appears I have Version 1.34

pastedImage_1.png

How do I update ICDPPCNEXUS?  I've tried using the CodeWarrior Updater and it says I'm up-to-date

pastedImage_2.png

0 件の賞賛
返信

5,020件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

you can download ICDPPCNEXUS from the link below and check, if it works.

ICDPPCNEXUS | In-Circuit Debugger for NXP MPC55xx/56xx/57xx & STMicroelectronics SPC5 | PEmicro 

Another possibility is contact PeMicro support directly and ask them, if they can provide you the newest version for CW2.10.

Regards,

Martin

0 件の賞賛
返信

5,020件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

I can see some download link at Product Details tab. Please see the figure below.

pastedImage_1.png

But from my point of view, it would be good, if you contact PeMicro support, describe your problem and ask them, what could be the best solution.

Regards,

Martin

0 件の賞賛
返信

4,367件の閲覧回数
smallyang
Contributor IV

你好,请问我的pemicro调试器输入install code 没有生成蓝色的registration code 是怎么回事呢

这是别人的界面

smallyang_0-1711185119092.pngsmallyang_0-1711185119092.png

 

 

这是我的界面

smallyang_1-1711185119423.pngsmallyang_1-1711185119423.png

 

 

0 件の賞賛
返信