Memory area address restriction with code warrior 10.6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Memory area address restriction with code warrior 10.6

1,554件の閲覧回数
tahirmahmood
Contributor I

I am getting the following error which doing RUN in code warrior 10.6. I am using MK10DN128. How can I remove this error.

 

152835_152835.pngpastedImage_0.png

ラベル(1)
0 件の賞賛
返信
1 返信

1,466件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Tahir

Could you please create a new bareboard project for MK10DN128?  Does CodeWarrior debugger work well with your board?

If not, please unsecure flash by mass ease as the attached doc.

In addition, CodeWarrior v10.6 is an old version, please upgrade to CW10.6.6.

Please first install CW10.6.4 which can be downloaded from:

CodeWarrior for Microcontrollers-Eclipse IDE|NXP

Its update v10.6.5 and v10.6.6 are also available at the same link.

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信