Max size memory tolerated for CodeWarrior in a trial version

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Max size memory tolerated for CodeWarrior in a trial version

1,251件の閲覧回数
karimaaissaoui
Contributor II

I will like to find out if it's possible, the max size memory tolerated for CodeWarrior in a trial version.

Thank you in advance.

ラベル(1)
0 件の賞賛
返信
1 返信

1,129件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Karima

Both Evaluation Edition and Special Edition are free.

The former works same as professional edition, but it has 30-day time restriction.

The latter has no time restriction, but it has C code size limit, for details, please refer to:

http://www.nxp.com/files/soft_dev_tools/doc/fact_sheet/950-00437.pdf

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

  ---------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信