MQX4.1 not detecting in CW10.5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX4.1 not detecting in CW10.5

ソリューションへジャンプ
3,404件の閲覧回数
madhukaravs
Contributor II

I have installed CW 10.5 and MQX4.1. But not able to create MQX project.

 

152662_152662.bmpScreen shot 1.bmp

ラベル(1)
1 解決策
3,085件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

from your screenshot, all the five items are color icons which means they are not fully installed

pastedImage_0.png

from the error messages, a certain item should be partly installed and has been recorded by CW.

I suggest you fully uninstall CW and remained install.

reinstall CW10.5, then install "MCU v10.5 Updates for MQX", "CW10.5 update". Please pay attention to the install sequence/

at last install MQX4.1.

see how it works?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
10 返答(返信)
3,085件の閲覧回数
madhukaravs
Contributor II

thank you ... i followed the same procedure in some other PC and it installed perfectly.....

( Even in my first PC its not , may be CCS i have installed. It might giving issue)

Thank you  :smileyhappy::smileyhappy::smileyhappy:

0 件の賞賛
返信
3,085件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome! :-)

0 件の賞賛
返信
3,085件の閲覧回数
madhukaravs
Contributor II

Can you tell me where exactly i can get MQTT header and neccesary files ? I want to MQTT for MQX.

0 件の賞賛
返信
3,085件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

As I know there is a known discussion regarding to MQTT, see

MQTT client libraryMQTT client library

if above thread can not help you, to separate different subject, can you please create a new thread for MQTT related question? Thanks!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,085件の閲覧回数
madhukaravs
Contributor II

thats really helpfull..

I forgot to menstio that im using GPRS modem(G620) and i need to implemet MQTT client .

0 件の賞賛
返信
3,086件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

from your screenshot, all the five items are color icons which means they are not fully installed

pastedImage_0.png

from the error messages, a certain item should be partly installed and has been recorded by CW.

I suggest you fully uninstall CW and remained install.

reinstall CW10.5, then install "MCU v10.5 Updates for MQX", "CW10.5 update". Please pay attention to the install sequence/

at last install MQX4.1.

see how it works?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,085件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

MQX 4.1 was developed to work with CW MCU v10.5. It has been tested and confirmed to work with CW MCU v10.6.

please

- uninstall your CW and MQX

- restart computer

- install CW10.5

- install CW10.5 update

- install MQX4.1

- restart computer

see how it works?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,085件の閲覧回数
madhukaravs
Contributor II

i tried but no use..... even i tried with different PC. but no use.

MQX3.8 is working fine. But MQX4.1 giving issue

0 件の賞賛
返信
3,085件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

did you install "MCU v10.5 Updates for MQX" as I highlight below? it's necessary.

pastedImage_1.png

Besides I also suggest you install other items I highlighted in purple.

MQX4.1 must be installed AFTER CW10.5 updates installed.

above steps work on many computers for us and customers. please double check.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,085件の閲覧回数
madhukaravs
Contributor II

I installed CW10.5 first

And now i tired to install the updates.

The option which are highlighted in purple, installed without any issue

but  the option highlighted in yellow color, giving issue.

Untitled.png

0 件の賞賛
返信