MPC8377 sample project creation fails with CW 10.4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8377 sample project creation fails with CW 10.4

ソリューションへジャンプ
3,695件の閲覧回数
juhalaukkanen
Contributor III

Hello.

 

I am not able to create a sample project with CodeWarrior 10.4 on Windows 7. After the creation wizard finishes nothing happens. Might be that some error output is somewhere? I am not avare of CW/Eclipse logging facilities.

 

Here's how to create a sample project

 

New -> Bareboard Project Wizard -> 83xx -> 8377 -> Application -> Finish

 

After Pressing that Finish button nothing happens, no project is generated.

 

Thanks.

ラベル(1)
1 解決策
3,432件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Juha Laukkanen,


In the workspace folder, there is a ".metadata" folder recording eclipse behavior, you could find .log into this folder, you also could attach it to us to do more investigation.

Thanks,

Yiping

元の投稿で解決策を見る

5 返答(返信)
3,432件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Juha Laukkanen,


The normal wizards should be like this


New -> Bareboard Project Wizard -> 83xx -> 8377 -> Application->Next(Debug Target Settings)->Next(Build Settings)->Next(Configurations)->Finish.

Please make sure you downloaded CodeWarrior 10.4 from CodeWarrior Dev Tools for Power Architecture|Freescale.

Please try to create a sample project in a new workspace.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,432件の閲覧回数
juhalaukkanen
Contributor III

I tried creating with following wizard flow

New -> Bareboard Project Wizard -> 83xx -> 8377 -> Application->Next(Debug Target Settings)->Next(Build Settings)->Next(Configurations)->Finish.

And into completely new and fresh workspace. Still doesn't work.

I noticed that project creation succeeds on different Win7 setup with CW10.4 where CW8.x and 10.4 are both installed parallel. Then I tried importing that generated sample project to the crippled Win7 CW10.4 setup where project generation fails. The imported project works flawlessly on the crippled Win7 CW10.4 (build, JTAG download, debug, etc). So only generation seems to fail on the crippled Win7 CW10.4.

Where can I see Eclipse logs what goes wrong with that wizard while generating the sample project? On Linux I know Eclipse outputs to console/stdout when launched from command line, but with Windows 7 I have no idea where messages go.

0 件の賞賛
返信
3,433件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Juha Laukkanen,


In the workspace folder, there is a ".metadata" folder recording eclipse behavior, you could find .log into this folder, you also could attach it to us to do more investigation.

Thanks,

Yiping

3,432件の閲覧回数
juhalaukkanen
Contributor III

OK now I did look at workspace\.metadata\.log and saw following line

!ENTRY com.freescale.core.ide.newprojectwizard 4 0 2015-01-16 09:44:09.624

!MESSAGE C:\User\Freescale\CodeWarrior PA V10.4.0\eclipse\..\PA\PA_Support\ewl\lib\libc_E300c4.a (The system cannot find the file specified)

!STACK 0

java.io.FileNotFoundException: C:\User\Freescale\CodeWarrior PA V10.4.0\eclipse\..\PA\PA_Support\ewl\lib\libc_E300c4.a (The system cannot find the file specified)

    at java.io.FileInputStream.open(Native Method)

    at java.io.FileInputStream.<init>(Unknown Source)

    at java.io.FileInputStream.<init>(Unknown Source)

    at com.freescale.core.ide.newprojectwizard.NewProjectCreator.createFileGroups(NewProjectCreator.java:737)

    at com.freescale.core.ide.newprojectwizard.NewProjectCreator.createProject(NewProjectCreator.java:408)

    at com.freescale.core.ide.newprojectwizard.NewProjectCreator.createProjects(NewProjectCreator.java:250)

    at com.freescale.core.ide.newprojectwizard.CWWizard.doRun(CWWizard.java:489)

    at com.freescale.core.ide.newprojectwizard.CWWizard$1$1$1.run(CWWizard.java:422)

    at org.eclipse.ui.actions.WorkspaceModifyDelegatingOperation.execute(WorkspaceModifyDelegatingOperation.java:69)

    at org.eclipse.ui.actions.WorkspaceModifyOperation$1.run(WorkspaceModifyOperation.java:106)

    at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2391)

    at org.eclipse.ui.actions.WorkspaceModifyOperation.run(WorkspaceModifyOperation.java:118)

    at org.eclipse.jface.operation.ModalContext.runInCurrentThread(ModalContext.java:464)

    at org.eclipse.jface.operation.ModalContext.run(ModalContext.java:372)

    at org.eclipse.jface.wizard.WizardDialog.run(WizardDialog.java:1031)

    at com.freescale.core.ide.newprojectwizard.CWWizard$1$1.run(CWWizard.java:432)

    at org.eclipse.ui.internal.UILockListener.doPendingWork(UILockListener.java:164)

    at org.eclipse.ui.internal.UISynchronizer$3.run(UISynchronizer.java:158)

    at org.eclipse.swt.widgets.RunnableLock.run(RunnableLock.java:35)

    at org.eclipse.swt.widgets.Synchronizer.runAsyncMessages(Synchronizer.java:155)

    at org.eclipse.swt.widgets.Display.runAsyncMessages(Display.java:4155)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3768)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3750)

    at org.eclipse.jface.operation.ModalContext$ModalContextThread.block(ModalContext.java:173)

    at org.eclipse.jface.operation.ModalContext.run(ModalContext.java:388)

    at org.eclipse.jface.wizard.WizardDialog.run(WizardDialog.java:1031)

    at com.freescale.core.ide.newprojectwizard.CWWizard.invokeRunnable(CWWizard.java:459)

    at com.freescale.core.ide.newprojectwizard.CWWizard.performFinish(CWWizard.java:323)

    at org.eclipse.jface.wizard.WizardDialog.finishPressed(WizardDialog.java:829)

    at org.eclipse.jface.wizard.WizardDialog.buttonPressed(WizardDialog.java:434)

    at org.eclipse.jface.dialogs.Dialog$2.widgetSelected(Dialog.java:624)

    at org.eclipse.swt.widgets.TypedListener.handleEvent(TypedListener.java:240)

    at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84)

    at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1053)

    at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:4180)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3765)

    at org.eclipse.jface.window.Window.runEventLoop(Window.java:825)

    at org.eclipse.jface.window.Window.open(Window.java:801)

    at org.eclipse.ui.actions.NewProjectAction.run(NewProjectAction.java:117)

    at org.eclipse.jface.action.Action.runWithEvent(Action.java:498)

    at org.eclipse.jface.action.ActionContributionItem.handleWidgetSelection(ActionContributionItem.java:584)

    at org.eclipse.jface.action.ActionContributionItem.access$2(ActionContributionItem.java:501)

    at org.eclipse.jface.action.ActionContributionItem$5.handleEvent(ActionContributionItem.java:411)

    at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84)

    at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1053)

    at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:4180)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3765)

    at org.eclipse.ui.internal.Workbench.runEventLoop(Workbench.java:2698)

    at org.eclipse.ui.internal.Workbench.runUI(Workbench.java:2662)

    at org.eclipse.ui.internal.Workbench.access$4(Workbench.java:2496)

    at org.eclipse.ui.internal.Workbench$5.run(Workbench.java:675)

    at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:332)

    at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:668)

    at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:149)

    at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:123)

    at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:196)

    at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:203)

    at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:82)

    at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:344)

    at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:179)

    at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)

    at sun.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)

    at sun.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)

    at java.lang.reflect.Method.invoke(Unknown Source)

    at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:623)

    at org.eclipse.equinox.launcher.Main.basicRun(Main.java:578)

    at org.eclipse.equinox.launcher.Main.run(Main.java:1411)

!ENTRY com.freescale.core.ide.newprojectwizard 4 0 2015-01-16 09:44:09.625

!MESSAGE C:\User\Freescale\CodeWarrior PA V10.4.0\eclipse\..\PA\PA_Support\ewl\lib\libc_E300c4.a (The system cannot find the file specified)

So I went to look that lib folder and noticed that some files were missing for some reason... So I just copied missing files from working installation and now it works even thought it still seems to output some errors to .log.

!ENTRY org.eclipse.cdt.core 4 0 2015-01-16 09:49:56.234

!MESSAGE Error: Element  does not exist.

!STACK 1

C Model Exception: C Model Status [Element  does not exist.]

    at org.eclipse.cdt.internal.core.model.PathEntryManager.getRawPathEntries(PathEntryManager.java:644)

    at org.eclipse.cdt.internal.core.model.PathEntryManager.getResolvedPathEntries(PathEntryManager.java:550)

    at org.eclipse.cdt.internal.core.model.PathEntryManager.getResolvedPathEntries(PathEntryManager.java:534)

    at org.eclipse.cdt.internal.core.model.PathEntryManager.getResolvedPathEntries(PathEntryManager.java:520)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreChangedOperation.executeOperation(PathEntryStoreChangedOperation.java:41)

    at org.eclipse.cdt.internal.core.model.CModelOperation.execute(CModelOperation.java:339)

    at org.eclipse.cdt.internal.core.model.CModelOperation.run(CModelOperation.java:602)

    at org.eclipse.cdt.internal.core.model.CModelOperation.runOperation(CModelOperation.java:630)

    at org.eclipse.cdt.internal.core.model.PathEntryManager.pathEntryStoreChanged(PathEntryManager.java:1303)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreProxy.notifyListeners(PathEntryStoreProxy.java:66)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreProxy.fireContentChangedEvent(PathEntryStoreProxy.java:59)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreProxy.postProcessProviderChange(PathEntryStoreProxy.java:145)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreProxy.doHandleEvent(PathEntryStoreProxy.java:153)

    at org.eclipse.cdt.internal.core.settings.model.AbstractCExtensionProxy.handleEvent(AbstractCExtensionProxy.java:153)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.notifyListeners(CProjectDescriptionManager.java:2371)

    at org.eclipse.cdt.internal.core.settings.model.SetCProjectDescriptionOperation.executeOperation(SetCProjectDescriptionOperation.java:141)

    at org.eclipse.cdt.internal.core.model.CModelOperation.execute(CModelOperation.java:339)

    at org.eclipse.cdt.internal.core.model.CModelOperation.run(CModelOperation.java:602)

    at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2391)

    at org.eclipse.cdt.internal.core.model.CModelOperation.runOperation(CModelOperation.java:633)

    at org.eclipse.cdt.internal.core.settings.model.AbstractCProjectDescriptionStorage.setProjectDescription(AbstractCProjectDescriptionStorage.java:203)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionStorageManager.setProjectDescription(CProjectDescriptionStorageManager.java:149)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:866)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:836)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:831)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptor$SerializingJob.serialize(CConfigBasedDescriptor.java:137)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptor.apply(CConfigBasedDescriptor.java:260)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptor.checkApply(CConfigBasedDescriptor.java:274)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptor.remove(CConfigBasedDescriptor.java:602)

    at org.eclipse.cdt.managedbuilder.internal.core.ManagedMakeProject.configure(ManagedMakeProject.java:49)

    at org.eclipse.cdt.internal.core.COwner.configure(COwner.java:42)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptorManager.updateDescriptor(CConfigBasedDescriptorManager.java:198)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptorManager.configure(CConfigBasedDescriptorManager.java:166)

    at org.eclipse.cdt.core.CCorePlugin.mapCProjectOwner(CCorePlugin.java:745)

    at org.eclipse.cdt.core.CCorePlugin$1.run(CCorePlugin.java:804)

    at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2391)

    at org.eclipse.cdt.core.CCorePlugin.createCProject(CCorePlugin.java:786)

    at com.freescale.core.ide.newprojectwizard.NewProjectCreator.createProjectResource(NewProjectCreator.java:569)

    at com.freescale.core.ide.newprojectwizard.NewProjectCreator.createProject(NewProjectCreator.java:379)

    at com.freescale.core.ide.newprojectwizard.NewProjectCreator.createProjects(NewProjectCreator.java:250)

    at com.freescale.core.ide.newprojectwizard.CWWizard.doRun(CWWizard.java:489)

    at com.freescale.core.ide.newprojectwizard.CWWizard$1$1$1.run(CWWizard.java:422)

    at org.eclipse.ui.actions.WorkspaceModifyDelegatingOperation.execute(WorkspaceModifyDelegatingOperation.java:69)

    at org.eclipse.ui.actions.WorkspaceModifyOperation$1.run(WorkspaceModifyOperation.java:106)

    at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2391)

    at org.eclipse.ui.actions.WorkspaceModifyOperation.run(WorkspaceModifyOperation.java:118)

    at org.eclipse.jface.operation.ModalContext.runInCurrentThread(ModalContext.java:464)

    at org.eclipse.jface.operation.ModalContext.run(ModalContext.java:372)

    at org.eclipse.jface.wizard.WizardDialog.run(WizardDialog.java:1031)

    at com.freescale.core.ide.newprojectwizard.CWWizard$1$1.run(CWWizard.java:432)

    at org.eclipse.ui.internal.UILockListener.doPendingWork(UILockListener.java:164)

    at org.eclipse.ui.internal.UISynchronizer$3.run(UISynchronizer.java:158)

    at org.eclipse.swt.widgets.RunnableLock.run(RunnableLock.java:35)

    at org.eclipse.swt.widgets.Synchronizer.runAsyncMessages(Synchronizer.java:155)

    at org.eclipse.swt.widgets.Display.runAsyncMessages(Display.java:4155)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3768)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3750)

    at org.eclipse.jface.operation.ModalContext$ModalContextThread.block(ModalContext.java:173)

    at org.eclipse.jface.operation.ModalContext.run(ModalContext.java:388)

    at org.eclipse.jface.wizard.WizardDialog.run(WizardDialog.java:1031)

    at com.freescale.core.ide.newprojectwizard.CWWizard.invokeRunnable(CWWizard.java:459)

    at com.freescale.core.ide.newprojectwizard.CWWizard.performFinish(CWWizard.java:323)

    at org.eclipse.jface.wizard.WizardDialog.finishPressed(WizardDialog.java:829)

    at org.eclipse.jface.wizard.WizardDialog.buttonPressed(WizardDialog.java:434)

    at org.eclipse.jface.dialogs.Dialog$2.widgetSelected(Dialog.java:624)

    at org.eclipse.swt.widgets.TypedListener.handleEvent(TypedListener.java:240)

    at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84)

    at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1053)

    at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:4180)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3765)

    at org.eclipse.jface.window.Window.runEventLoop(Window.java:825)

    at org.eclipse.jface.window.Window.open(Window.java:801)

    at org.eclipse.ui.actions.NewProjectAction.run(NewProjectAction.java:117)

    at org.eclipse.jface.action.Action.runWithEvent(Action.java:498)

    at org.eclipse.jface.action.ActionContributionItem.handleWidgetSelection(ActionContributionItem.java:584)

    at org.eclipse.jface.action.ActionContributionItem.access$2(ActionContributionItem.java:501)

    at org.eclipse.jface.action.ActionContributionItem$5.handleEvent(ActionContributionItem.java:411)

    at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84)

    at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1053)

    at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:4180)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3765)

    at org.eclipse.ui.internal.Workbench.runEventLoop(Workbench.java:2698)

    at org.eclipse.ui.internal.Workbench.runUI(Workbench.java:2662)

    at org.eclipse.ui.internal.Workbench.access$4(Workbench.java:2496)

    at org.eclipse.ui.internal.Workbench$5.run(Workbench.java:675)

    at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:332)

    at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:668)

    at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:149)

    at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:123)

    at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:196)

    at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:203)

    at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:82)

    at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:344)

    at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:179)

    at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)

    at sun.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)

    at sun.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)

    at java.lang.reflect.Method.invoke(Unknown Source)

    at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:623)

    at org.eclipse.equinox.launcher.Main.basicRun(Main.java:578)

    at org.eclipse.equinox.launcher.Main.run(Main.java:1411)

!SUBENTRY 1 org.eclipse.cdt.core 4 969 2015-01-16 09:49:56.235

!MESSAGE Element  does not exist.

!ENTRY org.eclipse.cdt.core 4 0 2015-01-16 09:49:56.242

!MESSAGE Error: Element  does not exist.

!STACK 1

C Model Exception: C Model Status [Element  does not exist.]

    at org.eclipse.cdt.internal.core.model.PathEntryManager.getRawPathEntries(PathEntryManager.java:644)

    at org.eclipse.cdt.internal.core.model.PathEntryManager.getResolvedPathEntries(PathEntryManager.java:550)

    at org.eclipse.cdt.internal.core.model.PathEntryManager.getResolvedPathEntries(PathEntryManager.java:534)

    at org.eclipse.cdt.internal.core.model.PathEntryManager.getResolvedPathEntries(PathEntryManager.java:520)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreChangedOperation.executeOperation(PathEntryStoreChangedOperation.java:41)

    at org.eclipse.cdt.internal.core.model.CModelOperation.execute(CModelOperation.java:339)

    at org.eclipse.cdt.internal.core.model.CModelOperation.run(CModelOperation.java:602)

    at org.eclipse.cdt.internal.core.model.CModelOperation.runOperation(CModelOperation.java:630)

    at org.eclipse.cdt.internal.core.model.PathEntryManager.pathEntryStoreChanged(PathEntryManager.java:1303)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreProxy.notifyListeners(PathEntryStoreProxy.java:66)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreProxy.pathEntryStoreChanged(PathEntryStoreProxy.java:110)

    at org.eclipse.cdt.internal.core.model.DefaultPathEntryStore.fireContentChangedEvent(DefaultPathEntryStore.java:392)

    at org.eclipse.cdt.internal.core.model.DefaultPathEntryStore.descriptorChanged(DefaultPathEntryStore.java:368)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptorManager$2.run(CConfigBasedDescriptorManager.java:589)

    at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:42)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptorManager.notifyListeners(CConfigBasedDescriptorManager.java:580)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptorManager.doHandleEvent(CConfigBasedDescriptorManager.java:543)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptorManager.access$0(CConfigBasedDescriptorManager.java:464)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptorManager$1.handleEvent(CConfigBasedDescriptorManager.java:444)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.notifyListeners(CProjectDescriptionManager.java:2371)

    at org.eclipse.cdt.internal.core.settings.model.SetCProjectDescriptionOperation.executeOperation(SetCProjectDescriptionOperation.java:141)

    at org.eclipse.cdt.internal.core.model.CModelOperation.execute(CModelOperation.java:339)

    at org.eclipse.cdt.internal.core.model.CModelOperation.run(CModelOperation.java:602)

    at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2391)

    at org.eclipse.cdt.internal.core.model.CModelOperation.runOperation(CModelOperation.java:633)

    at org.eclipse.cdt.internal.core.settings.model.AbstractCProjectDescriptionStorage.setProjectDescription(AbstractCProjectDescriptionStorage.java:203)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionStorageManager.setProjectDescription(CProjectDescriptionStorageManager.java:149)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:866)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:836)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:831)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptor$SerializingJob.serialize(CConfigBasedDescriptor.java:137)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptor.apply(CConfigBasedDescriptor.java:260)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptor.checkApply(CConfigBasedDescriptor.java:274)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptor.remove(CConfigBasedDescriptor.java:602)

    at org.eclipse.cdt.managedbuilder.internal.core.ManagedMakeProject.configure(ManagedMakeProject.java:51)

    at org.eclipse.cdt.internal.core.COwner.configure(COwner.java:42)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptorManager.updateDescriptor(CConfigBasedDescriptorManager.java:198)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptorManager.configure(CConfigBasedDescriptorManager.java:166)

    at org.eclipse.cdt.core.CCorePlugin.mapCProjectOwner(CCorePlugin.java:745)

    at org.eclipse.cdt.core.CCorePlugin$1.run(CCorePlugin.java:804)

    at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2391)

    at org.eclipse.cdt.core.CCorePlugin.createCProject(CCorePlugin.java:786)

    at com.freescale.core.ide.newprojectwizard.NewProjectCreator.createProjectResource(NewProjectCreator.java:569)

    at com.freescale.core.ide.newprojectwizard.NewProjectCreator.createProject(NewProjectCreator.java:379)

    at com.freescale.core.ide.newprojectwizard.NewProjectCreator.createProjects(NewProjectCreator.java:250)

    at com.freescale.core.ide.newprojectwizard.CWWizard.doRun(CWWizard.java:489)

    at com.freescale.core.ide.newprojectwizard.CWWizard$1$1$1.run(CWWizard.java:422)

    at org.eclipse.ui.actions.WorkspaceModifyDelegatingOperation.execute(WorkspaceModifyDelegatingOperation.java:69)

    at org.eclipse.ui.actions.WorkspaceModifyOperation$1.run(WorkspaceModifyOperation.java:106)

    at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2391)

    at org.eclipse.ui.actions.WorkspaceModifyOperation.run(WorkspaceModifyOperation.java:118)

    at org.eclipse.jface.operation.ModalContext.runInCurrentThread(ModalContext.java:464)

    at org.eclipse.jface.operation.ModalContext.run(ModalContext.java:372)

    at org.eclipse.jface.wizard.WizardDialog.run(WizardDialog.java:1031)

    at com.freescale.core.ide.newprojectwizard.CWWizard$1$1.run(CWWizard.java:432)

    at org.eclipse.ui.internal.UILockListener.doPendingWork(UILockListener.java:164)

    at org.eclipse.ui.internal.UISynchronizer$3.run(UISynchronizer.java:158)

    at org.eclipse.swt.widgets.RunnableLock.run(RunnableLock.java:35)

    at org.eclipse.swt.widgets.Synchronizer.runAsyncMessages(Synchronizer.java:155)

    at org.eclipse.swt.widgets.Display.runAsyncMessages(Display.java:4155)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3768)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3750)

    at org.eclipse.jface.operation.ModalContext$ModalContextThread.block(ModalContext.java:173)

    at org.eclipse.jface.operation.ModalContext.run(ModalContext.java:388)

    at org.eclipse.jface.wizard.WizardDialog.run(WizardDialog.java:1031)

    at com.freescale.core.ide.newprojectwizard.CWWizard.invokeRunnable(CWWizard.java:459)

    at com.freescale.core.ide.newprojectwizard.CWWizard.performFinish(CWWizard.java:323)

    at org.eclipse.jface.wizard.WizardDialog.finishPressed(WizardDialog.java:829)

    at org.eclipse.jface.wizard.WizardDialog.buttonPressed(WizardDialog.java:434)

    at org.eclipse.jface.dialogs.Dialog$2.widgetSelected(Dialog.java:624)

    at org.eclipse.swt.widgets.TypedListener.handleEvent(TypedListener.java:240)

    at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84)

    at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1053)

    at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:4180)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3765)

    at org.eclipse.jface.window.Window.runEventLoop(Window.java:825)

    at org.eclipse.jface.window.Window.open(Window.java:801)

    at org.eclipse.ui.actions.NewProjectAction.run(NewProjectAction.java:117)

    at org.eclipse.jface.action.Action.runWithEvent(Action.java:498)

    at org.eclipse.jface.action.ActionContributionItem.handleWidgetSelection(ActionContributionItem.java:584)

    at org.eclipse.jface.action.ActionContributionItem.access$2(ActionContributionItem.java:501)

    at org.eclipse.jface.action.ActionContributionItem$5.handleEvent(ActionContributionItem.java:411)

    at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84)

    at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1053)

    at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:4180)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3765)

    at org.eclipse.ui.internal.Workbench.runEventLoop(Workbench.java:2698)

    at org.eclipse.ui.internal.Workbench.runUI(Workbench.java:2662)

    at org.eclipse.ui.internal.Workbench.access$4(Workbench.java:2496)

    at org.eclipse.ui.internal.Workbench$5.run(Workbench.java:675)

    at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:332)

    at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:668)

    at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:149)

    at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:123)

    at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:196)

    at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:203)

    at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:82)

    at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:344)

    at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:179)

    at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)

    at sun.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)

    at sun.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)

    at java.lang.reflect.Method.invoke(Unknown Source)

    at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:623)

    at org.eclipse.equinox.launcher.Main.basicRun(Main.java:578)

    at org.eclipse.equinox.launcher.Main.run(Main.java:1411)

!SUBENTRY 1 org.eclipse.cdt.core 4 969 2015-01-16 09:49:56.242

!MESSAGE Element  does not exist.

!ENTRY org.eclipse.cdt.core 4 0 2015-01-16 09:49:56.243

!MESSAGE Error: Element  does not exist.

!STACK 1

C Model Exception: C Model Status [Element  does not exist.]

    at org.eclipse.cdt.internal.core.model.PathEntryManager.getRawPathEntries(PathEntryManager.java:644)

    at org.eclipse.cdt.internal.core.model.PathEntryManager.getResolvedPathEntries(PathEntryManager.java:550)

    at org.eclipse.cdt.internal.core.model.PathEntryManager.getResolvedPathEntries(PathEntryManager.java:534)

    at org.eclipse.cdt.internal.core.model.PathEntryManager.getResolvedPathEntries(PathEntryManager.java:520)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreChangedOperation.executeOperation(PathEntryStoreChangedOperation.java:41)

    at org.eclipse.cdt.internal.core.model.CModelOperation.execute(CModelOperation.java:339)

    at org.eclipse.cdt.internal.core.model.CModelOperation.run(CModelOperation.java:602)

    at org.eclipse.cdt.internal.core.model.CModelOperation.runOperation(CModelOperation.java:630)

    at org.eclipse.cdt.internal.core.model.PathEntryManager.pathEntryStoreChanged(PathEntryManager.java:1303)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreProxy.notifyListeners(PathEntryStoreProxy.java:66)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreProxy.fireContentChangedEvent(PathEntryStoreProxy.java:59)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreProxy.postProcessProviderChange(PathEntryStoreProxy.java:145)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreProxy.doHandleEvent(PathEntryStoreProxy.java:153)

    at org.eclipse.cdt.internal.core.settings.model.AbstractCExtensionProxy.handleEvent(AbstractCExtensionProxy.java:153)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.notifyListeners(CProjectDescriptionManager.java:2371)

    at org.eclipse.cdt.internal.core.settings.model.SetCProjectDescriptionOperation.executeOperation(SetCProjectDescriptionOperation.java:141)

    at org.eclipse.cdt.internal.core.model.CModelOperation.execute(CModelOperation.java:339)

    at org.eclipse.cdt.internal.core.model.CModelOperation.run(CModelOperation.java:602)

    at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2391)

    at org.eclipse.cdt.internal.core.model.CModelOperation.runOperation(CModelOperation.java:633)

    at org.eclipse.cdt.internal.core.settings.model.AbstractCProjectDescriptionStorage.setProjectDescription(AbstractCProjectDescriptionStorage.java:203)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionStorageManager.setProjectDescription(CProjectDescriptionStorageManager.java:149)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:866)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:836)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:831)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptor$SerializingJob.serialize(CConfigBasedDescriptor.java:137)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptor.apply(CConfigBasedDescriptor.java:260)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptor.checkApply(CConfigBasedDescriptor.java:274)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptor.remove(CConfigBasedDescriptor.java:602)

    at org.eclipse.cdt.managedbuilder.internal.core.ManagedMakeProject.configure(ManagedMakeProject.java:51)

    at org.eclipse.cdt.internal.core.COwner.configure(COwner.java:42)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptorManager.updateDescriptor(CConfigBasedDescriptorManager.java:198)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptorManager.configure(CConfigBasedDescriptorManager.java:166)

    at org.eclipse.cdt.core.CCorePlugin.mapCProjectOwner(CCorePlugin.java:745)

    at org.eclipse.cdt.core.CCorePlugin$1.run(CCorePlugin.java:804)

    at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2391)

    at org.eclipse.cdt.core.CCorePlugin.createCProject(CCorePlugin.java:786)

    at com.freescale.core.ide.newprojectwizard.NewProjectCreator.createProjectResource(NewProjectCreator.java:569)

    at com.freescale.core.ide.newprojectwizard.NewProjectCreator.createProject(NewProjectCreator.java:379)

    at com.freescale.core.ide.newprojectwizard.NewProjectCreator.createProjects(NewProjectCreator.java:250)

    at com.freescale.core.ide.newprojectwizard.CWWizard.doRun(CWWizard.java:489)

    at com.freescale.core.ide.newprojectwizard.CWWizard$1$1$1.run(CWWizard.java:422)

    at org.eclipse.ui.actions.WorkspaceModifyDelegatingOperation.execute(WorkspaceModifyDelegatingOperation.java:69)

    at org.eclipse.ui.actions.WorkspaceModifyOperation$1.run(WorkspaceModifyOperation.java:106)

    at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2391)

    at org.eclipse.ui.actions.WorkspaceModifyOperation.run(WorkspaceModifyOperation.java:118)

    at org.eclipse.jface.operation.ModalContext.runInCurrentThread(ModalContext.java:464)

    at org.eclipse.jface.operation.ModalContext.run(ModalContext.java:372)

    at org.eclipse.jface.wizard.WizardDialog.run(WizardDialog.java:1031)

    at com.freescale.core.ide.newprojectwizard.CWWizard$1$1.run(CWWizard.java:432)

    at org.eclipse.ui.internal.UILockListener.doPendingWork(UILockListener.java:164)

    at org.eclipse.ui.internal.UISynchronizer$3.run(UISynchronizer.java:158)

    at org.eclipse.swt.widgets.RunnableLock.run(RunnableLock.java:35)

    at org.eclipse.swt.widgets.Synchronizer.runAsyncMessages(Synchronizer.java:155)

    at org.eclipse.swt.widgets.Display.runAsyncMessages(Display.java:4155)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3768)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3750)

    at org.eclipse.jface.operation.ModalContext$ModalContextThread.block(ModalContext.java:173)

    at org.eclipse.jface.operation.ModalContext.run(ModalContext.java:388)

    at org.eclipse.jface.wizard.WizardDialog.run(WizardDialog.java:1031)

    at com.freescale.core.ide.newprojectwizard.CWWizard.invokeRunnable(CWWizard.java:459)

    at com.freescale.core.ide.newprojectwizard.CWWizard.performFinish(CWWizard.java:323)

    at org.eclipse.jface.wizard.WizardDialog.finishPressed(WizardDialog.java:829)

    at org.eclipse.jface.wizard.WizardDialog.buttonPressed(WizardDialog.java:434)

    at org.eclipse.jface.dialogs.Dialog$2.widgetSelected(Dialog.java:624)

    at org.eclipse.swt.widgets.TypedListener.handleEvent(TypedListener.java:240)

    at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84)

    at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1053)

    at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:4180)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3765)

    at org.eclipse.jface.window.Window.runEventLoop(Window.java:825)

    at org.eclipse.jface.window.Window.open(Window.java:801)

    at org.eclipse.ui.actions.NewProjectAction.run(NewProjectAction.java:117)

    at org.eclipse.jface.action.Action.runWithEvent(Action.java:498)

    at org.eclipse.jface.action.ActionContributionItem.handleWidgetSelection(ActionContributionItem.java:584)

    at org.eclipse.jface.action.ActionContributionItem.access$2(ActionContributionItem.java:501)

    at org.eclipse.jface.action.ActionContributionItem$5.handleEvent(ActionContributionItem.java:411)

    at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84)

    at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1053)

    at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:4180)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3765)

    at org.eclipse.ui.internal.Workbench.runEventLoop(Workbench.java:2698)

    at org.eclipse.ui.internal.Workbench.runUI(Workbench.java:2662)

    at org.eclipse.ui.internal.Workbench.access$4(Workbench.java:2496)

    at org.eclipse.ui.internal.Workbench$5.run(Workbench.java:675)

    at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:332)

    at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:668)

    at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:149)

    at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:123)

    at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:196)

    at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:203)

    at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:82)

    at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:344)

    at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:179)

    at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)

    at sun.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)

    at sun.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)

    at java.lang.reflect.Method.invoke(Unknown Source)

    at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:623)

    at org.eclipse.equinox.launcher.Main.basicRun(Main.java:578)

    at org.eclipse.equinox.launcher.Main.run(Main.java:1411)

!SUBENTRY 1 org.eclipse.cdt.core 4 969 2015-01-16 09:49:56.243

!MESSAGE Element  does not exist.

!ENTRY org.eclipse.cdt.core 1 0 2015-01-16 09:49:59.661

!MESSAGE Indexed 'mpc8377test-core00' (3 sources, 53 headers) in 0,89 sec: 801 declarations; 1 518 references; 2 unresolved inclusions; 2 syntax errors; 2 unresolved names (0,09 %)

0 件の賞賛
返信
3,432件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Juha Laukkanen,

Probably you have already seen the error message in your log as the following.

!MESSAGE C:\User\Freescale\CodeWarrior PA V10.4.0\eclipse\..\PA\PA_Support\ewl\lib\libc_E300c4.a (The system cannot find the file specified)

The file libc_E300c4.a should exist in the normal CodeWarrior installation, but it is missing in your installation directory. Maybe you need to install CodeWarrior 10.4 again.

Thanks,

Yiping

0 件の賞賛
返信