MPC8377 sample project creation fails with CW 10.4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8377 sample project creation fails with CW 10.4

Jump to solution
3,720 Views
juhalaukkanen
Contributor III

Hello.

 

I am not able to create a sample project with CodeWarrior 10.4 on Windows 7. After the creation wizard finishes nothing happens. Might be that some error output is somewhere? I am not avare of CW/Eclipse logging facilities.

 

Here's how to create a sample project

 

New -> Bareboard Project Wizard -> 83xx -> 8377 -> Application -> Finish

 

After Pressing that Finish button nothing happens, no project is generated.

 

Thanks.

Labels (1)
1 Solution
3,457 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Juha Laukkanen,


In the workspace folder, there is a ".metadata" folder recording eclipse behavior, you could find .log into this folder, you also could attach it to us to do more investigation.

Thanks,

Yiping

View solution in original post

5 Replies
3,457 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Juha Laukkanen,


The normal wizards should be like this


New -> Bareboard Project Wizard -> 83xx -> 8377 -> Application->Next(Debug Target Settings)->Next(Build Settings)->Next(Configurations)->Finish.

Please make sure you downloaded CodeWarrior 10.4 from CodeWarrior Dev Tools for Power Architecture|Freescale.

Please try to create a sample project in a new workspace.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,457 Views
juhalaukkanen
Contributor III

I tried creating with following wizard flow

New -> Bareboard Project Wizard -> 83xx -> 8377 -> Application->Next(Debug Target Settings)->Next(Build Settings)->Next(Configurations)->Finish.

And into completely new and fresh workspace. Still doesn't work.

I noticed that project creation succeeds on different Win7 setup with CW10.4 where CW8.x and 10.4 are both installed parallel. Then I tried importing that generated sample project to the crippled Win7 CW10.4 setup where project generation fails. The imported project works flawlessly on the crippled Win7 CW10.4 (build, JTAG download, debug, etc). So only generation seems to fail on the crippled Win7 CW10.4.

Where can I see Eclipse logs what goes wrong with that wizard while generating the sample project? On Linux I know Eclipse outputs to console/stdout when launched from command line, but with Windows 7 I have no idea where messages go.

0 Kudos
Reply
3,458 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Juha Laukkanen,


In the workspace folder, there is a ".metadata" folder recording eclipse behavior, you could find .log into this folder, you also could attach it to us to do more investigation.

Thanks,

Yiping

3,457 Views
juhalaukkanen
Contributor III

OK now I did look at workspace\.metadata\.log and saw following line

!ENTRY com.freescale.core.ide.newprojectwizard 4 0 2015-01-16 09:44:09.624

!MESSAGE C:\User\Freescale\CodeWarrior PA V10.4.0\eclipse\..\PA\PA_Support\ewl\lib\libc_E300c4.a (The system cannot find the file specified)

!STACK 0

java.io.FileNotFoundException: C:\User\Freescale\CodeWarrior PA V10.4.0\eclipse\..\PA\PA_Support\ewl\lib\libc_E300c4.a (The system cannot find the file specified)

    at java.io.FileInputStream.open(Native Method)

    at java.io.FileInputStream.<init>(Unknown Source)

    at java.io.FileInputStream.<init>(Unknown Source)

    at com.freescale.core.ide.newprojectwizard.NewProjectCreator.createFileGroups(NewProjectCreator.java:737)

    at com.freescale.core.ide.newprojectwizard.NewProjectCreator.createProject(NewProjectCreator.java:408)

    at com.freescale.core.ide.newprojectwizard.NewProjectCreator.createProjects(NewProjectCreator.java:250)

    at com.freescale.core.ide.newprojectwizard.CWWizard.doRun(CWWizard.java:489)

    at com.freescale.core.ide.newprojectwizard.CWWizard$1$1$1.run(CWWizard.java:422)

    at org.eclipse.ui.actions.WorkspaceModifyDelegatingOperation.execute(WorkspaceModifyDelegatingOperation.java:69)

    at org.eclipse.ui.actions.WorkspaceModifyOperation$1.run(WorkspaceModifyOperation.java:106)

    at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2391)

    at org.eclipse.ui.actions.WorkspaceModifyOperation.run(WorkspaceModifyOperation.java:118)

    at org.eclipse.jface.operation.ModalContext.runInCurrentThread(ModalContext.java:464)

    at org.eclipse.jface.operation.ModalContext.run(ModalContext.java:372)

    at org.eclipse.jface.wizard.WizardDialog.run(WizardDialog.java:1031)

    at com.freescale.core.ide.newprojectwizard.CWWizard$1$1.run(CWWizard.java:432)

    at org.eclipse.ui.internal.UILockListener.doPendingWork(UILockListener.java:164)

    at org.eclipse.ui.internal.UISynchronizer$3.run(UISynchronizer.java:158)

    at org.eclipse.swt.widgets.RunnableLock.run(RunnableLock.java:35)

    at org.eclipse.swt.widgets.Synchronizer.runAsyncMessages(Synchronizer.java:155)

    at org.eclipse.swt.widgets.Display.runAsyncMessages(Display.java:4155)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3768)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3750)

    at org.eclipse.jface.operation.ModalContext$ModalContextThread.block(ModalContext.java:173)

    at org.eclipse.jface.operation.ModalContext.run(ModalContext.java:388)

    at org.eclipse.jface.wizard.WizardDialog.run(WizardDialog.java:1031)

    at com.freescale.core.ide.newprojectwizard.CWWizard.invokeRunnable(CWWizard.java:459)

    at com.freescale.core.ide.newprojectwizard.CWWizard.performFinish(CWWizard.java:323)

    at org.eclipse.jface.wizard.WizardDialog.finishPressed(WizardDialog.java:829)

    at org.eclipse.jface.wizard.WizardDialog.buttonPressed(WizardDialog.java:434)

    at org.eclipse.jface.dialogs.Dialog$2.widgetSelected(Dialog.java:624)

    at org.eclipse.swt.widgets.TypedListener.handleEvent(TypedListener.java:240)

    at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84)

    at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1053)

    at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:4180)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3765)

    at org.eclipse.jface.window.Window.runEventLoop(Window.java:825)

    at org.eclipse.jface.window.Window.open(Window.java:801)

    at org.eclipse.ui.actions.NewProjectAction.run(NewProjectAction.java:117)

    at org.eclipse.jface.action.Action.runWithEvent(Action.java:498)

    at org.eclipse.jface.action.ActionContributionItem.handleWidgetSelection(ActionContributionItem.java:584)

    at org.eclipse.jface.action.ActionContributionItem.access$2(ActionContributionItem.java:501)

    at org.eclipse.jface.action.ActionContributionItem$5.handleEvent(ActionContributionItem.java:411)

    at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84)

    at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1053)

    at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:4180)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3765)

    at org.eclipse.ui.internal.Workbench.runEventLoop(Workbench.java:2698)

    at org.eclipse.ui.internal.Workbench.runUI(Workbench.java:2662)

    at org.eclipse.ui.internal.Workbench.access$4(Workbench.java:2496)

    at org.eclipse.ui.internal.Workbench$5.run(Workbench.java:675)

    at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:332)

    at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:668)

    at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:149)

    at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:123)

    at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:196)

    at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:203)

    at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:82)

    at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:344)

    at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:179)

    at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)

    at sun.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)

    at sun.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)

    at java.lang.reflect.Method.invoke(Unknown Source)

    at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:623)

    at org.eclipse.equinox.launcher.Main.basicRun(Main.java:578)

    at org.eclipse.equinox.launcher.Main.run(Main.java:1411)

!ENTRY com.freescale.core.ide.newprojectwizard 4 0 2015-01-16 09:44:09.625

!MESSAGE C:\User\Freescale\CodeWarrior PA V10.4.0\eclipse\..\PA\PA_Support\ewl\lib\libc_E300c4.a (The system cannot find the file specified)

So I went to look that lib folder and noticed that some files were missing for some reason... So I just copied missing files from working installation and now it works even thought it still seems to output some errors to .log.

!ENTRY org.eclipse.cdt.core 4 0 2015-01-16 09:49:56.234

!MESSAGE Error: Element  does not exist.

!STACK 1

C Model Exception: C Model Status [Element  does not exist.]

    at org.eclipse.cdt.internal.core.model.PathEntryManager.getRawPathEntries(PathEntryManager.java:644)

    at org.eclipse.cdt.internal.core.model.PathEntryManager.getResolvedPathEntries(PathEntryManager.java:550)

    at org.eclipse.cdt.internal.core.model.PathEntryManager.getResolvedPathEntries(PathEntryManager.java:534)

    at org.eclipse.cdt.internal.core.model.PathEntryManager.getResolvedPathEntries(PathEntryManager.java:520)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreChangedOperation.executeOperation(PathEntryStoreChangedOperation.java:41)

    at org.eclipse.cdt.internal.core.model.CModelOperation.execute(CModelOperation.java:339)

    at org.eclipse.cdt.internal.core.model.CModelOperation.run(CModelOperation.java:602)

    at org.eclipse.cdt.internal.core.model.CModelOperation.runOperation(CModelOperation.java:630)

    at org.eclipse.cdt.internal.core.model.PathEntryManager.pathEntryStoreChanged(PathEntryManager.java:1303)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreProxy.notifyListeners(PathEntryStoreProxy.java:66)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreProxy.fireContentChangedEvent(PathEntryStoreProxy.java:59)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreProxy.postProcessProviderChange(PathEntryStoreProxy.java:145)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreProxy.doHandleEvent(PathEntryStoreProxy.java:153)

    at org.eclipse.cdt.internal.core.settings.model.AbstractCExtensionProxy.handleEvent(AbstractCExtensionProxy.java:153)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.notifyListeners(CProjectDescriptionManager.java:2371)

    at org.eclipse.cdt.internal.core.settings.model.SetCProjectDescriptionOperation.executeOperation(SetCProjectDescriptionOperation.java:141)

    at org.eclipse.cdt.internal.core.model.CModelOperation.execute(CModelOperation.java:339)

    at org.eclipse.cdt.internal.core.model.CModelOperation.run(CModelOperation.java:602)

    at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2391)

    at org.eclipse.cdt.internal.core.model.CModelOperation.runOperation(CModelOperation.java:633)

    at org.eclipse.cdt.internal.core.settings.model.AbstractCProjectDescriptionStorage.setProjectDescription(AbstractCProjectDescriptionStorage.java:203)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionStorageManager.setProjectDescription(CProjectDescriptionStorageManager.java:149)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:866)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:836)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:831)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptor$SerializingJob.serialize(CConfigBasedDescriptor.java:137)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptor.apply(CConfigBasedDescriptor.java:260)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptor.checkApply(CConfigBasedDescriptor.java:274)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptor.remove(CConfigBasedDescriptor.java:602)

    at org.eclipse.cdt.managedbuilder.internal.core.ManagedMakeProject.configure(ManagedMakeProject.java:49)

    at org.eclipse.cdt.internal.core.COwner.configure(COwner.java:42)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptorManager.updateDescriptor(CConfigBasedDescriptorManager.java:198)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptorManager.configure(CConfigBasedDescriptorManager.java:166)

    at org.eclipse.cdt.core.CCorePlugin.mapCProjectOwner(CCorePlugin.java:745)

    at org.eclipse.cdt.core.CCorePlugin$1.run(CCorePlugin.java:804)

    at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2391)

    at org.eclipse.cdt.core.CCorePlugin.createCProject(CCorePlugin.java:786)

    at com.freescale.core.ide.newprojectwizard.NewProjectCreator.createProjectResource(NewProjectCreator.java:569)

    at com.freescale.core.ide.newprojectwizard.NewProjectCreator.createProject(NewProjectCreator.java:379)

    at com.freescale.core.ide.newprojectwizard.NewProjectCreator.createProjects(NewProjectCreator.java:250)

    at com.freescale.core.ide.newprojectwizard.CWWizard.doRun(CWWizard.java:489)

    at com.freescale.core.ide.newprojectwizard.CWWizard$1$1$1.run(CWWizard.java:422)

    at org.eclipse.ui.actions.WorkspaceModifyDelegatingOperation.execute(WorkspaceModifyDelegatingOperation.java:69)

    at org.eclipse.ui.actions.WorkspaceModifyOperation$1.run(WorkspaceModifyOperation.java:106)

    at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2391)

    at org.eclipse.ui.actions.WorkspaceModifyOperation.run(WorkspaceModifyOperation.java:118)

    at org.eclipse.jface.operation.ModalContext.runInCurrentThread(ModalContext.java:464)

    at org.eclipse.jface.operation.ModalContext.run(ModalContext.java:372)

    at org.eclipse.jface.wizard.WizardDialog.run(WizardDialog.java:1031)

    at com.freescale.core.ide.newprojectwizard.CWWizard$1$1.run(CWWizard.java:432)

    at org.eclipse.ui.internal.UILockListener.doPendingWork(UILockListener.java:164)

    at org.eclipse.ui.internal.UISynchronizer$3.run(UISynchronizer.java:158)

    at org.eclipse.swt.widgets.RunnableLock.run(RunnableLock.java:35)

    at org.eclipse.swt.widgets.Synchronizer.runAsyncMessages(Synchronizer.java:155)

    at org.eclipse.swt.widgets.Display.runAsyncMessages(Display.java:4155)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3768)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3750)

    at org.eclipse.jface.operation.ModalContext$ModalContextThread.block(ModalContext.java:173)

    at org.eclipse.jface.operation.ModalContext.run(ModalContext.java:388)

    at org.eclipse.jface.wizard.WizardDialog.run(WizardDialog.java:1031)

    at com.freescale.core.ide.newprojectwizard.CWWizard.invokeRunnable(CWWizard.java:459)

    at com.freescale.core.ide.newprojectwizard.CWWizard.performFinish(CWWizard.java:323)

    at org.eclipse.jface.wizard.WizardDialog.finishPressed(WizardDialog.java:829)

    at org.eclipse.jface.wizard.WizardDialog.buttonPressed(WizardDialog.java:434)

    at org.eclipse.jface.dialogs.Dialog$2.widgetSelected(Dialog.java:624)

    at org.eclipse.swt.widgets.TypedListener.handleEvent(TypedListener.java:240)

    at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84)

    at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1053)

    at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:4180)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3765)

    at org.eclipse.jface.window.Window.runEventLoop(Window.java:825)

    at org.eclipse.jface.window.Window.open(Window.java:801)

    at org.eclipse.ui.actions.NewProjectAction.run(NewProjectAction.java:117)

    at org.eclipse.jface.action.Action.runWithEvent(Action.java:498)

    at org.eclipse.jface.action.ActionContributionItem.handleWidgetSelection(ActionContributionItem.java:584)

    at org.eclipse.jface.action.ActionContributionItem.access$2(ActionContributionItem.java:501)

    at org.eclipse.jface.action.ActionContributionItem$5.handleEvent(ActionContributionItem.java:411)

    at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84)

    at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1053)

    at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:4180)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3765)

    at org.eclipse.ui.internal.Workbench.runEventLoop(Workbench.java:2698)

    at org.eclipse.ui.internal.Workbench.runUI(Workbench.java:2662)

    at org.eclipse.ui.internal.Workbench.access$4(Workbench.java:2496)

    at org.eclipse.ui.internal.Workbench$5.run(Workbench.java:675)

    at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:332)

    at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:668)

    at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:149)

    at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:123)

    at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:196)

    at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:203)

    at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:82)

    at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:344)

    at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:179)

    at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)

    at sun.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)

    at sun.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)

    at java.lang.reflect.Method.invoke(Unknown Source)

    at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:623)

    at org.eclipse.equinox.launcher.Main.basicRun(Main.java:578)

    at org.eclipse.equinox.launcher.Main.run(Main.java:1411)

!SUBENTRY 1 org.eclipse.cdt.core 4 969 2015-01-16 09:49:56.235

!MESSAGE Element  does not exist.

!ENTRY org.eclipse.cdt.core 4 0 2015-01-16 09:49:56.242

!MESSAGE Error: Element  does not exist.

!STACK 1

C Model Exception: C Model Status [Element  does not exist.]

    at org.eclipse.cdt.internal.core.model.PathEntryManager.getRawPathEntries(PathEntryManager.java:644)

    at org.eclipse.cdt.internal.core.model.PathEntryManager.getResolvedPathEntries(PathEntryManager.java:550)

    at org.eclipse.cdt.internal.core.model.PathEntryManager.getResolvedPathEntries(PathEntryManager.java:534)

    at org.eclipse.cdt.internal.core.model.PathEntryManager.getResolvedPathEntries(PathEntryManager.java:520)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreChangedOperation.executeOperation(PathEntryStoreChangedOperation.java:41)

    at org.eclipse.cdt.internal.core.model.CModelOperation.execute(CModelOperation.java:339)

    at org.eclipse.cdt.internal.core.model.CModelOperation.run(CModelOperation.java:602)

    at org.eclipse.cdt.internal.core.model.CModelOperation.runOperation(CModelOperation.java:630)

    at org.eclipse.cdt.internal.core.model.PathEntryManager.pathEntryStoreChanged(PathEntryManager.java:1303)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreProxy.notifyListeners(PathEntryStoreProxy.java:66)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreProxy.pathEntryStoreChanged(PathEntryStoreProxy.java:110)

    at org.eclipse.cdt.internal.core.model.DefaultPathEntryStore.fireContentChangedEvent(DefaultPathEntryStore.java:392)

    at org.eclipse.cdt.internal.core.model.DefaultPathEntryStore.descriptorChanged(DefaultPathEntryStore.java:368)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptorManager$2.run(CConfigBasedDescriptorManager.java:589)

    at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:42)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptorManager.notifyListeners(CConfigBasedDescriptorManager.java:580)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptorManager.doHandleEvent(CConfigBasedDescriptorManager.java:543)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptorManager.access$0(CConfigBasedDescriptorManager.java:464)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptorManager$1.handleEvent(CConfigBasedDescriptorManager.java:444)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.notifyListeners(CProjectDescriptionManager.java:2371)

    at org.eclipse.cdt.internal.core.settings.model.SetCProjectDescriptionOperation.executeOperation(SetCProjectDescriptionOperation.java:141)

    at org.eclipse.cdt.internal.core.model.CModelOperation.execute(CModelOperation.java:339)

    at org.eclipse.cdt.internal.core.model.CModelOperation.run(CModelOperation.java:602)

    at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2391)

    at org.eclipse.cdt.internal.core.model.CModelOperation.runOperation(CModelOperation.java:633)

    at org.eclipse.cdt.internal.core.settings.model.AbstractCProjectDescriptionStorage.setProjectDescription(AbstractCProjectDescriptionStorage.java:203)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionStorageManager.setProjectDescription(CProjectDescriptionStorageManager.java:149)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:866)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:836)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:831)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptor$SerializingJob.serialize(CConfigBasedDescriptor.java:137)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptor.apply(CConfigBasedDescriptor.java:260)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptor.checkApply(CConfigBasedDescriptor.java:274)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptor.remove(CConfigBasedDescriptor.java:602)

    at org.eclipse.cdt.managedbuilder.internal.core.ManagedMakeProject.configure(ManagedMakeProject.java:51)

    at org.eclipse.cdt.internal.core.COwner.configure(COwner.java:42)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptorManager.updateDescriptor(CConfigBasedDescriptorManager.java:198)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptorManager.configure(CConfigBasedDescriptorManager.java:166)

    at org.eclipse.cdt.core.CCorePlugin.mapCProjectOwner(CCorePlugin.java:745)

    at org.eclipse.cdt.core.CCorePlugin$1.run(CCorePlugin.java:804)

    at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2391)

    at org.eclipse.cdt.core.CCorePlugin.createCProject(CCorePlugin.java:786)

    at com.freescale.core.ide.newprojectwizard.NewProjectCreator.createProjectResource(NewProjectCreator.java:569)

    at com.freescale.core.ide.newprojectwizard.NewProjectCreator.createProject(NewProjectCreator.java:379)

    at com.freescale.core.ide.newprojectwizard.NewProjectCreator.createProjects(NewProjectCreator.java:250)

    at com.freescale.core.ide.newprojectwizard.CWWizard.doRun(CWWizard.java:489)

    at com.freescale.core.ide.newprojectwizard.CWWizard$1$1$1.run(CWWizard.java:422)

    at org.eclipse.ui.actions.WorkspaceModifyDelegatingOperation.execute(WorkspaceModifyDelegatingOperation.java:69)

    at org.eclipse.ui.actions.WorkspaceModifyOperation$1.run(WorkspaceModifyOperation.java:106)

    at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2391)

    at org.eclipse.ui.actions.WorkspaceModifyOperation.run(WorkspaceModifyOperation.java:118)

    at org.eclipse.jface.operation.ModalContext.runInCurrentThread(ModalContext.java:464)

    at org.eclipse.jface.operation.ModalContext.run(ModalContext.java:372)

    at org.eclipse.jface.wizard.WizardDialog.run(WizardDialog.java:1031)

    at com.freescale.core.ide.newprojectwizard.CWWizard$1$1.run(CWWizard.java:432)

    at org.eclipse.ui.internal.UILockListener.doPendingWork(UILockListener.java:164)

    at org.eclipse.ui.internal.UISynchronizer$3.run(UISynchronizer.java:158)

    at org.eclipse.swt.widgets.RunnableLock.run(RunnableLock.java:35)

    at org.eclipse.swt.widgets.Synchronizer.runAsyncMessages(Synchronizer.java:155)

    at org.eclipse.swt.widgets.Display.runAsyncMessages(Display.java:4155)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3768)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3750)

    at org.eclipse.jface.operation.ModalContext$ModalContextThread.block(ModalContext.java:173)

    at org.eclipse.jface.operation.ModalContext.run(ModalContext.java:388)

    at org.eclipse.jface.wizard.WizardDialog.run(WizardDialog.java:1031)

    at com.freescale.core.ide.newprojectwizard.CWWizard.invokeRunnable(CWWizard.java:459)

    at com.freescale.core.ide.newprojectwizard.CWWizard.performFinish(CWWizard.java:323)

    at org.eclipse.jface.wizard.WizardDialog.finishPressed(WizardDialog.java:829)

    at org.eclipse.jface.wizard.WizardDialog.buttonPressed(WizardDialog.java:434)

    at org.eclipse.jface.dialogs.Dialog$2.widgetSelected(Dialog.java:624)

    at org.eclipse.swt.widgets.TypedListener.handleEvent(TypedListener.java:240)

    at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84)

    at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1053)

    at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:4180)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3765)

    at org.eclipse.jface.window.Window.runEventLoop(Window.java:825)

    at org.eclipse.jface.window.Window.open(Window.java:801)

    at org.eclipse.ui.actions.NewProjectAction.run(NewProjectAction.java:117)

    at org.eclipse.jface.action.Action.runWithEvent(Action.java:498)

    at org.eclipse.jface.action.ActionContributionItem.handleWidgetSelection(ActionContributionItem.java:584)

    at org.eclipse.jface.action.ActionContributionItem.access$2(ActionContributionItem.java:501)

    at org.eclipse.jface.action.ActionContributionItem$5.handleEvent(ActionContributionItem.java:411)

    at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84)

    at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1053)

    at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:4180)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3765)

    at org.eclipse.ui.internal.Workbench.runEventLoop(Workbench.java:2698)

    at org.eclipse.ui.internal.Workbench.runUI(Workbench.java:2662)

    at org.eclipse.ui.internal.Workbench.access$4(Workbench.java:2496)

    at org.eclipse.ui.internal.Workbench$5.run(Workbench.java:675)

    at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:332)

    at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:668)

    at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:149)

    at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:123)

    at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:196)

    at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:203)

    at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:82)

    at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:344)

    at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:179)

    at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)

    at sun.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)

    at sun.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)

    at java.lang.reflect.Method.invoke(Unknown Source)

    at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:623)

    at org.eclipse.equinox.launcher.Main.basicRun(Main.java:578)

    at org.eclipse.equinox.launcher.Main.run(Main.java:1411)

!SUBENTRY 1 org.eclipse.cdt.core 4 969 2015-01-16 09:49:56.242

!MESSAGE Element  does not exist.

!ENTRY org.eclipse.cdt.core 4 0 2015-01-16 09:49:56.243

!MESSAGE Error: Element  does not exist.

!STACK 1

C Model Exception: C Model Status [Element  does not exist.]

    at org.eclipse.cdt.internal.core.model.PathEntryManager.getRawPathEntries(PathEntryManager.java:644)

    at org.eclipse.cdt.internal.core.model.PathEntryManager.getResolvedPathEntries(PathEntryManager.java:550)

    at org.eclipse.cdt.internal.core.model.PathEntryManager.getResolvedPathEntries(PathEntryManager.java:534)

    at org.eclipse.cdt.internal.core.model.PathEntryManager.getResolvedPathEntries(PathEntryManager.java:520)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreChangedOperation.executeOperation(PathEntryStoreChangedOperation.java:41)

    at org.eclipse.cdt.internal.core.model.CModelOperation.execute(CModelOperation.java:339)

    at org.eclipse.cdt.internal.core.model.CModelOperation.run(CModelOperation.java:602)

    at org.eclipse.cdt.internal.core.model.CModelOperation.runOperation(CModelOperation.java:630)

    at org.eclipse.cdt.internal.core.model.PathEntryManager.pathEntryStoreChanged(PathEntryManager.java:1303)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreProxy.notifyListeners(PathEntryStoreProxy.java:66)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreProxy.fireContentChangedEvent(PathEntryStoreProxy.java:59)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreProxy.postProcessProviderChange(PathEntryStoreProxy.java:145)

    at org.eclipse.cdt.internal.core.model.PathEntryStoreProxy.doHandleEvent(PathEntryStoreProxy.java:153)

    at org.eclipse.cdt.internal.core.settings.model.AbstractCExtensionProxy.handleEvent(AbstractCExtensionProxy.java:153)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.notifyListeners(CProjectDescriptionManager.java:2371)

    at org.eclipse.cdt.internal.core.settings.model.SetCProjectDescriptionOperation.executeOperation(SetCProjectDescriptionOperation.java:141)

    at org.eclipse.cdt.internal.core.model.CModelOperation.execute(CModelOperation.java:339)

    at org.eclipse.cdt.internal.core.model.CModelOperation.run(CModelOperation.java:602)

    at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2391)

    at org.eclipse.cdt.internal.core.model.CModelOperation.runOperation(CModelOperation.java:633)

    at org.eclipse.cdt.internal.core.settings.model.AbstractCProjectDescriptionStorage.setProjectDescription(AbstractCProjectDescriptionStorage.java:203)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionStorageManager.setProjectDescription(CProjectDescriptionStorageManager.java:149)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:866)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:836)

    at org.eclipse.cdt.internal.core.settings.model.CProjectDescriptionManager.setProjectDescription(CProjectDescriptionManager.java:831)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptor$SerializingJob.serialize(CConfigBasedDescriptor.java:137)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptor.apply(CConfigBasedDescriptor.java:260)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptor.checkApply(CConfigBasedDescriptor.java:274)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptor.remove(CConfigBasedDescriptor.java:602)

    at org.eclipse.cdt.managedbuilder.internal.core.ManagedMakeProject.configure(ManagedMakeProject.java:51)

    at org.eclipse.cdt.internal.core.COwner.configure(COwner.java:42)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptorManager.updateDescriptor(CConfigBasedDescriptorManager.java:198)

    at org.eclipse.cdt.internal.core.CConfigBasedDescriptorManager.configure(CConfigBasedDescriptorManager.java:166)

    at org.eclipse.cdt.core.CCorePlugin.mapCProjectOwner(CCorePlugin.java:745)

    at org.eclipse.cdt.core.CCorePlugin$1.run(CCorePlugin.java:804)

    at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2391)

    at org.eclipse.cdt.core.CCorePlugin.createCProject(CCorePlugin.java:786)

    at com.freescale.core.ide.newprojectwizard.NewProjectCreator.createProjectResource(NewProjectCreator.java:569)

    at com.freescale.core.ide.newprojectwizard.NewProjectCreator.createProject(NewProjectCreator.java:379)

    at com.freescale.core.ide.newprojectwizard.NewProjectCreator.createProjects(NewProjectCreator.java:250)

    at com.freescale.core.ide.newprojectwizard.CWWizard.doRun(CWWizard.java:489)

    at com.freescale.core.ide.newprojectwizard.CWWizard$1$1$1.run(CWWizard.java:422)

    at org.eclipse.ui.actions.WorkspaceModifyDelegatingOperation.execute(WorkspaceModifyDelegatingOperation.java:69)

    at org.eclipse.ui.actions.WorkspaceModifyOperation$1.run(WorkspaceModifyOperation.java:106)

    at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2391)

    at org.eclipse.ui.actions.WorkspaceModifyOperation.run(WorkspaceModifyOperation.java:118)

    at org.eclipse.jface.operation.ModalContext.runInCurrentThread(ModalContext.java:464)

    at org.eclipse.jface.operation.ModalContext.run(ModalContext.java:372)

    at org.eclipse.jface.wizard.WizardDialog.run(WizardDialog.java:1031)

    at com.freescale.core.ide.newprojectwizard.CWWizard$1$1.run(CWWizard.java:432)

    at org.eclipse.ui.internal.UILockListener.doPendingWork(UILockListener.java:164)

    at org.eclipse.ui.internal.UISynchronizer$3.run(UISynchronizer.java:158)

    at org.eclipse.swt.widgets.RunnableLock.run(RunnableLock.java:35)

    at org.eclipse.swt.widgets.Synchronizer.runAsyncMessages(Synchronizer.java:155)

    at org.eclipse.swt.widgets.Display.runAsyncMessages(Display.java:4155)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3768)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3750)

    at org.eclipse.jface.operation.ModalContext$ModalContextThread.block(ModalContext.java:173)

    at org.eclipse.jface.operation.ModalContext.run(ModalContext.java:388)

    at org.eclipse.jface.wizard.WizardDialog.run(WizardDialog.java:1031)

    at com.freescale.core.ide.newprojectwizard.CWWizard.invokeRunnable(CWWizard.java:459)

    at com.freescale.core.ide.newprojectwizard.CWWizard.performFinish(CWWizard.java:323)

    at org.eclipse.jface.wizard.WizardDialog.finishPressed(WizardDialog.java:829)

    at org.eclipse.jface.wizard.WizardDialog.buttonPressed(WizardDialog.java:434)

    at org.eclipse.jface.dialogs.Dialog$2.widgetSelected(Dialog.java:624)

    at org.eclipse.swt.widgets.TypedListener.handleEvent(TypedListener.java:240)

    at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84)

    at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1053)

    at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:4180)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3765)

    at org.eclipse.jface.window.Window.runEventLoop(Window.java:825)

    at org.eclipse.jface.window.Window.open(Window.java:801)

    at org.eclipse.ui.actions.NewProjectAction.run(NewProjectAction.java:117)

    at org.eclipse.jface.action.Action.runWithEvent(Action.java:498)

    at org.eclipse.jface.action.ActionContributionItem.handleWidgetSelection(ActionContributionItem.java:584)

    at org.eclipse.jface.action.ActionContributionItem.access$2(ActionContributionItem.java:501)

    at org.eclipse.jface.action.ActionContributionItem$5.handleEvent(ActionContributionItem.java:411)

    at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:84)

    at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1053)

    at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:4180)

    at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3765)

    at org.eclipse.ui.internal.Workbench.runEventLoop(Workbench.java:2698)

    at org.eclipse.ui.internal.Workbench.runUI(Workbench.java:2662)

    at org.eclipse.ui.internal.Workbench.access$4(Workbench.java:2496)

    at org.eclipse.ui.internal.Workbench$5.run(Workbench.java:675)

    at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:332)

    at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:668)

    at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:149)

    at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:123)

    at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:196)

    at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:203)

    at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:82)

    at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:344)

    at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:179)

    at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)

    at sun.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)

    at sun.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)

    at java.lang.reflect.Method.invoke(Unknown Source)

    at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:623)

    at org.eclipse.equinox.launcher.Main.basicRun(Main.java:578)

    at org.eclipse.equinox.launcher.Main.run(Main.java:1411)

!SUBENTRY 1 org.eclipse.cdt.core 4 969 2015-01-16 09:49:56.243

!MESSAGE Element  does not exist.

!ENTRY org.eclipse.cdt.core 1 0 2015-01-16 09:49:59.661

!MESSAGE Indexed 'mpc8377test-core00' (3 sources, 53 headers) in 0,89 sec: 801 declarations; 1 518 references; 2 unresolved inclusions; 2 syntax errors; 2 unresolved names (0,09 %)

0 Kudos
Reply
3,457 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Juha Laukkanen,

Probably you have already seen the error message in your log as the following.

!MESSAGE C:\User\Freescale\CodeWarrior PA V10.4.0\eclipse\..\PA\PA_Support\ewl\lib\libc_E300c4.a (The system cannot find the file specified)

The file libc_E300c4.a should exist in the normal CodeWarrior installation, but it is missing in your installation directory. Maybe you need to install CodeWarrior 10.4 again.

Thanks,

Yiping

0 Kudos
Reply