MPC55XX Codewarrior Linker symbols cant be accessed...Stack paint

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC55XX Codewarrior Linker symbols cant be accessed...Stack paint

3,212 次查看
mechalec
Contributor I

Hi all,

 

This is my first post, so I hope it is clear and concise but also in the correct section.

 

I am doing some development on a MPC5534, using Freescales Codewarrior compiler.

 

I am trying to implement a stack paint algorithm, so that I can determine my stack usage at runtime.

 

My problem lies in the fact that I cannot access the linker generated symbols that are present in the ".lcf".

 

The compiler/linker error:

C:/Freescale/CW MCU v10.4/MCU/PA_Tools/Command_Line_Tools/mwldeppc|Linker|Error

>Small data relocation (109) in function 'vStackInit'

>in referencing file 'stack_c.obj'

>requires that symbol '_stack_addr'

>in symbol definition file 'linker generated symbol'

 

The function below is a simplification of my implementation so that you can get the "idea" of what I am doing.

There is no need to correct the algorithm (Yes, I know it is corrupting any existing values on the stack), but any help

as to the  syntax required to access the symbol "_stack_addr" would be greatly appreciated.

 

 

#define STACK_VALUE 0x55AA55AAul

 

void vStackInit( void );

extern uint32_t _stack_addr;

 

void vStackInit( void )

{

  unsigned int u32IntIndex = 0u;

  unsigned int *pu32Index = (unsigned int *)(_stack_addr);

 

  for(u32IntIndex = 0ul; u32IntIndex < 0x8000ul; u32IntIndex++ ) {

  pu32Index[u32IntIndex] = STACK_VALUE;

  }

}

 

Any help would be greatly appreciated.

Thanks

标签 (1)
0 项奖励
回复
3 回复数

2,679 次查看
DavidS
NXP Employee
NXP Employee

Hi Scott.

Haven't used the MPC5534 or tool set but the Kinetis device with CW10.x can access the linker script variable with following declaration in a "C" file"

const uchar __FLASHX_START_ADDR[];

Later in "C" file it is used with following way:

(uint_32) __FLASHX_START_ADDR

Hope this helps.

Regards,

David


0 项奖励
回复

2,679 次查看
mechalec
Contributor I

Thanks for the feedback, its really helpful. I will try compile and link with that and see if it pulls the correct value.

Regarding your declaration,  are you missing "extern"?

0 项奖励
回复

2,679 次查看
trytohelp
NXP Employee
NXP Employee

Hi,

for my understanding you could use the following.

in main.c file:

extern unsigned long _stack_addr[];

int main(void) {

  volatile int i = 0;

  unsigned long* StackStartAddr;

  StackStartAddr = _stack_addr;

in lcf file:

_stack_addr = ADDR(stack)+SIZEOF(stack);

I can build it without problem on my side.

However I don't have board to test it.

Pascal

0 项奖励
回复