MK70FN1M0VMJ12 device and code warrior as IDE 

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK70FN1M0VMJ12 device and code warrior as IDE 

1,070 Views
ankurchauhan
Contributor I

i'm using MK70FN1M0VMJ12 device and code warrior as IDE when i'm tring to run the code in ram its telling to update the bootload software. Is there any setting which i have to do.

Labels (1)
0 Kudos
Reply
1 Reply

965 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Ankur Chauhan,

Is this the message you get?

pastedImage_0.png

If yes, then you need to unplug the USB cable and place a jumper on the J10 connector in your tower K70 board and connect the USB cable again, this way the OSJTAG will enter to bootloader mode and the latest firmware will be programmed.

After the firmware has been updated you should see a window like this:

pastedImage_1.png

Now you should unplug the USB cable, remove the jumper from the J10 connector and connect the USB cable again.

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply