Log Window in CodeWarrior for ColdFire 7.2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Log Window in CodeWarrior for ColdFire 7.2

2,517 次查看
sahilgandhi
Contributor I

Hi,

 

I am trying to create a "Hello world!" applications for MQX52259.

 

In my application I have a printf statement, which is supposed to write the string on the Log Window as per the help documentation of IDE. I have also verified that the Debugger Settings has the Log System Messages is enabled.

 

So, ideally the Log Window should appear when I debug my program. But it is not appearing. Can you guys help with some troubleshooting steps?

 

Thanks in advance.

 

-sahil

标签 (1)
标记 (3)
0 项奖励
回复
3 回复数

2,456 次查看
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. CodeWarrior Development Tools ) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community. 

0 项奖励
回复

2,456 次查看
sahilgandhi
Contributor I

Moved it. Thanks for the suggestion

0 项奖励
回复

2,456 次查看
trytohelp
NXP Employee
NXP Employee

Problem has been logged under Service Request process.

Regards

Pascal

0 项奖励
回复