Link Order View-code warrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Link Order View-code warrior

2,860件の閲覧回数
georgemathew
Contributor II


The Link Order view of the Project window shows information about
how the IDE will compile or link the final output file for the project's current build
target.
The IDE links the files in order from top to bottom. For example, if file B depends on
file A, make sure that the Link Order view lists file B below file A.

 

what it means

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,659件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

The IDE links the files in order from top to bottom in CW "Link Order" tab.

the file on the top is linked before the files on the bottom.

thus with this link order,  the variable/function in the prior linked file will be recognized first.

"link order" defines a priority that searching variable/function in files.


Have a great day,
Jennie Zhang

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,659件の閲覧回数
georgemathew
Contributor II

if the link order is wrong, is it results in wrong output?

0 件の賞賛
返信

2,659件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

yes.

0 件の賞賛
返信

2,659件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi George,

Could you tell us which MCU and CodeWarrior version are you using?

Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信

2,659件の閲覧回数
georgemathew
Contributor II

codewarrior 5.1,  controller-MC9S12A128

0 件の賞賛
返信