LS1046A-FRWY system hangs when CodeWarrior connects

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046A-FRWY system hangs when CodeWarrior connects

2,034 Views
mindchasers
Contributor III

Hello,

I'm running the LS1046A Yocto SDK (5.4.3+g134788b16485). It boots fine and mounts its rootfs from the SD Card. When CodeWarrior connects, I get the following message on the terminal and then the terminal hangs.

"EXT4-fs (mmcblk0p3): re-mounted. Opts: (null)"

If I run rootfs from a RAM disk, the system seems to run fine with CodeWarrior.

I'm looking for suggestions on how to resolve this problem. Thank you.

0 Kudos
Reply
1 Reply

2,029 Views
yipingwang
NXP TechSupport
NXP TechSupport

Do you want to use CodeWarrior to connect to the target board to do Linux Kernel debugging?

If yes, please refer to CodeWarrior configuration in section 3 in this document.

https://community.nxp.com/t5/CodeWarrior-for-QorIQ-Knowledge/Use-CodeWarrior-for-ARMv8-to-Debug-U-bo...

0 Kudos
Reply