LS1021ATWR : Lauterbatch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1021ATWR : Lauterbatch

1,473 Views
amolshrotri
Contributor II


Hello,

 

I am trying to connect Lauterbach with LS1021ATWR, But getting error on SYSTEM.UP as "debug port fail".

 

I am using below commands

SYSTEM.CPU CORTEXA7MPCORE

SYSTEM.CONFIG DAPIRPRE 8.

SYSTEM.CONFIG DAPDRPRE 1.

SYSTEM.Option ResBreak OFF

CORE.ASSIGN 1.

SYSTEM.Up

Labels (1)
0 Kudos
Reply
1 Reply

1,319 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello AMOL SHROTRI,

For Lauterbach and Trace32 problem, you's better contact LAUTERBACH company LAUTERBACH DEVELOPMENT TOOLS.

For LS1021ATWR, make sure there is valid RCW on the target board,  if no, you could use hard-coded RCW.

Switch settings for LS1021A TWR X3 - PROC REV 1.0

SW2 : 0x8F = 1000 1111  

SW3 : 0x61 = 0110 0001

Switch settings fro LS1021A TWR X3 - PROC REV 2.0

SW2 : 0x8F = 1000 1111  

SW3 : 0x65 = 0110 0101

To enable CMSIS-DAP you have to change SW2[8] = 0


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply