LS1021A Rev2 Processor Connection On Custom Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1021A Rev2 Processor Connection On Custom Board

1,551件の閲覧回数
erdemyanar
Contributor I

Hi,

 

I am trying to connect on LS1021A processor which i implemented on my custom board. I got "CCS can not connected " error during connection. I attached detailed error zip.

 

######################################################################

Dikkat:

 

Bu elektronik posta mesaji kisisel ve ozeldir. Eger size

gonderilmediyse lutfen gondericiyi bilgilendirip mesaji siliniz.

Firmamiza gelen ve giden mesajlar virus taramasindan gecirilmekte,

guvenlik nedeni ile kontrol edilerek saklanmaktadir. Mesajdaki

gorusler ve bakis acisi gondericiye ait olup Aselsan A.S. resmi

gorusu olmak zorunda degildir.

 

######################################################################

Attention:

 

This e-mail message is privileged and confidential. If you are

not the intended recipient please delete the message and notify

the sender. E-mails to and from the company are monitored for

operational reasons and in accordance with lawful business practices.

Any views or opinions presented are solely those of the author and

do not necessarily represent the views of the company.

 

######################################################################

Original Attachment has been moved to: 201611210821_DiagnosticInfo.zip

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,454件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Erdem YANAR,

It seems that there is problem with your CodeWarrior installation.

Would you please download CodeWarrior from CodeWarrior® Development Tools for ARMv7|NXP , and reinstall it.


Have a great day,
Yiping

0 件の賞賛
返信

1,454件の閲覧回数
addiyi
NXP Employee
NXP Employee

What is the version of CodeWarrior?

Adrian

0 件の賞賛
返信