LM_NOTTHISHOST

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LM_NOTTHISHOST

1,998 Views
Shirley
Contributor I

It shows up in license error/detail window every time the CW10 is opened. But I'm able to build the project, have not try the debug mode yet.

I have node lock license, Win7 OS.

Anybody has the same problem?

Labels (1)
0 Kudos
Reply
1 Reply

1,609 Views
trytohelp
NXP Employee
NXP Employee

Hi,

Can you have a look to

    USBdongle license is not running for CW for PA V10.4 and MCU V10.4 (sometimes) -> "LM_NOTTHISHOST...

This is may be similar problem.


Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply