L4025: This limited version allows only 32768 bytes of C code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

L4025: This limited version allows only 32768 bytes of C code

ソリューションへジャンプ
6,103件の閲覧回数
mithunbharadwaj
Contributor I

L4025: This limited version allows only 32768 bytes of C code

 

I have 8 functions which need to be integrated into an existing C code.

 

I am able to call 5 of the 8 in buildDebug mode without errors.

 

But i get the above mentioned error when i call one more function.

 

Is this a limitation of my tool???

 

I am using CodeWarrior IDE Version 5.9.0  Build 5294

 

If i comment the code inside the 3 functions, i am still not able to link in debug mode, but links in release mode.

 

The code size comes up to 32520 when i comment the code inside the 3 functions.

 

Please help.

ラベル(1)
0 件の賞賛
返信
1 解決策
4,744件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

i wonder you use CW for HCS12(x) special edition which has 32k C object code size limit.

you need purchase license to allow more code size.

I have sent you evaluation license via SR to MITHUN0702@GMAIL.COM  for your test purpose.

hope this helps!

==================================

this answer is for you. if it helps, please click on "correct answer " button. thanks!

Best Regards,

Jennie

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
4,745件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

i wonder you use CW for HCS12(x) special edition which has 32k C object code size limit.

you need purchase license to allow more code size.

I have sent you evaluation license via SR to MITHUN0702@GMAIL.COM  for your test purpose.

hope this helps!

==================================

this answer is for you. if it helps, please click on "correct answer " button. thanks!

Best Regards,

Jennie

0 件の賞賛
返信
4,744件の閲覧回数
hiramrayotorres
Contributor I

Hi ZhangJennie , i am currently having the same issue regarding the compilation of a project bigger than 32K in the special edition for HCS12(x)  , could you please send me the evaluation license please? i would deeply appreciate it. Hrayotorres@gmail.com

Thanks in advance!

0 件の賞賛
返信
4,744件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

next time you have the same license request I suggest you submit your case into NXP supporting system, please follow below steps:
1) Go to http://www.nxp.com/support/sales-and-support:SUPPORTHOME.
2) On the bottom of the page under Submit New Issues, click Hardware & Software.
3) Register with your business email to access NXP technical online support.
4) A verification email will be sent to your account. Click the link embedded in that email to verify your access.
5) On the NXP online support page, select Contact Support from the top menu and click “submit a new case” to start the process.

119802_119802.pngpastedImage_0.png

thanks!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
4,744件の閲覧回数
mithunbharadwaj
Contributor I

Hello,

The evaluation license worked well.

Can you please provide me a extension of the license?

I am in the process of making arrangements for purchasing. It will take some time.

in the meanwhile can you please provide the evaluation license for an additional month?

0 件の賞賛
返信
4,744件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Mithum,

I have sent you answer via service request.

Best Regards,

Zhang Jun

0 件の賞賛
返信