KIT MPXY8300A

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KIT MPXY8300A

跳至解决方案
2,852 次查看
riccardocescato
Contributor I

Hi,

I'm using CodeWarrior 10.6 on window 8. I bought a KIT MPXY8300A but I have many problem with the code.

 

When I create a new project for the MPXY8300 family, the program doesn't generate the .h files where the functions described in the datasheet are implemented and

also the .h files for interrupts. In this way I can't write the code for my kit!

 

How can I do to create a new project with all these files??

 

Thank you!

标签 (1)
0 项奖励
回复
1 解答
2,741 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

hi Riccardo,

the file such as reims_firm_io_ES2.h is not CW system file. this file can not generated by CW automatically.

reims_firm_io_ES2.h is from a demo project, we can use it but CW can't create it.

=====================================================

this answer is for you. if it helps, please click on "correct answer " button. thanks!

Best Regards,

Jennie

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,742 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

hi Riccardo,

the file such as reims_firm_io_ES2.h is not CW system file. this file can not generated by CW automatically.

reims_firm_io_ES2.h is from a demo project, we can use it but CW can't create it.

=====================================================

this answer is for you. if it helps, please click on "correct answer " button. thanks!

Best Regards,

Jennie

0 项奖励
回复
2,741 次查看
riccardocescato
Contributor I

Ok I undestand. So, how can I create a new project from the demo project?

Because I have a problem with the hidef.h file that there isn't inside the project but it uses that file!

0 项奖励
回复