KIT MPXY8300A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KIT MPXY8300A

Jump to solution
2,914 Views
riccardocescato
Contributor I

Hi,

I'm using CodeWarrior 10.6 on window 8. I bought a KIT MPXY8300A but I have many problem with the code.

 

When I create a new project for the MPXY8300 family, the program doesn't generate the .h files where the functions described in the datasheet are implemented and

also the .h files for interrupts. In this way I can't write the code for my kit!

 

How can I do to create a new project with all these files??

 

Thank you!

Labels (1)
0 Kudos
Reply
1 Solution
2,803 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hi Riccardo,

the file such as reims_firm_io_ES2.h is not CW system file. this file can not generated by CW automatically.

reims_firm_io_ES2.h is from a demo project, we can use it but CW can't create it.

=====================================================

this answer is for you. if it helps, please click on "correct answer " button. thanks!

Best Regards,

Jennie

View solution in original post

0 Kudos
Reply
2 Replies
2,804 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hi Riccardo,

the file such as reims_firm_io_ES2.h is not CW system file. this file can not generated by CW automatically.

reims_firm_io_ES2.h is from a demo project, we can use it but CW can't create it.

=====================================================

this answer is for you. if it helps, please click on "correct answer " button. thanks!

Best Regards,

Jennie

0 Kudos
Reply
2,803 Views
riccardocescato
Contributor I

Ok I undestand. So, how can I create a new project from the demo project?

Because I have a problem with the hidef.h file that there isn't inside the project but it uses that file!

0 Kudos
Reply