K60 Baremetal Project Code Size Error: `.text' will not fit in region `m_text'

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K60 Baremetal Project Code Size Error: `.text' will not fit in region `m_text'

跳至解决方案
2,167 次查看
broccolee
Contributor III

Hi, 

 

I am using TWR-K60N512, with PK60DN512Z VMD10 chip and Codewarrior 10.5. I definitely have issues with the size of my code, I have about 50 source and header files in my source folder. About half of them are freemaster stuff, so I won't modify that. 

 

I'm wondering if anybody could:

1) Show me how to increase the maximum allowable code size, if at all possible, for baremetal projects .

2) Tell me if there's a way to display the part of my baremetal project code that is taking up too much memory so I can optimize it accordingly.

 

Here's the error I received:

c:/freescale/cw mcu v10.5/cross_tools/arm-none-eabi-gcc-4_7_3/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/bin/ld.exe: i2c.elf section `.text' will not fit in region `m_text'
c:/freescale/cw mcu v10.5/cross_tools/arm-none-eabi-gcc-4_7_3/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/bin/ld.exe: section .data loaded at [20000000,2000019b] overlaps section .text loaded at [1fff01e0,20001507]
c:/freescale/cw mcu v10.5/cross_tools/arm-none-eabi-gcc-4_7_3/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/bin/ld.exe: region `m_text' overflowed by 5384 bytes 
collect2.exe: error: ld returned 1 exit status
mingw32-make: *** [i2c.elf] Error 1

 

I have also attached a file with '.ld' format, which has some memory info for your reference.

 

Thanks.

Original Attachment has been moved to: PK60N512_ram.ld.zip

标签 (1)
0 项奖励
回复
1 解答
1,948 次查看
BlackNight
NXP Employee
NXP Employee

For 1) The allowed code size depends on your microcontroller (amount of on chip FLASH memory). The 512 variant has 512 KByte, so if you really need more, you need a bigger device with more FLASH. But what you could do otherwise is to turn on code size optimization in the compiler settings, this should reduce your code size by a bit.

For 2) You can report the code/data size for each object file, see https://mcuoneclipse.com/2014/07/13/listing-code-and-data-size-for-each-source-file-with-gnu-and-ecl... 

I hope this helps,

Erich

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,949 次查看
BlackNight
NXP Employee
NXP Employee

For 1) The allowed code size depends on your microcontroller (amount of on chip FLASH memory). The 512 variant has 512 KByte, so if you really need more, you need a bigger device with more FLASH. But what you could do otherwise is to turn on code size optimization in the compiler settings, this should reduce your code size by a bit.

For 2) You can report the code/data size for each object file, see https://mcuoneclipse.com/2014/07/13/listing-code-and-data-size-for-each-source-file-with-gnu-and-ecl... 

I hope this helps,

Erich

0 项奖励
回复
1,948 次查看
broccolee
Contributor III

Thank you, Sir! I turned on the code size optimization option and it reduced my codes size significantly!

0 项奖励
回复