Issue while debugging with Optimizer OFF

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Issue while debugging with Optimizer OFF

跳至解决方案
2,252 次查看
kpanchamia
Contributor I

Setup:

CW10.5

K61FX512

Code runs from Ext RAM

TraceLink & Multilink

 

When I turn optimizer ON ( =1), code runs alright.

If it is turned OFF ( = 0), code compiles properly & even the debugger session is invoked. But as soon as I do a "step over" at __init_registers in __thumb_startup, it shows "No source available". "Step into" does work but only for few instructions.

 

Also at this time, in the memory view, all the values are reset to 0x00. (Maybe - DDR connection broken somehow???)

 

I started a session with Tracelink too, but the trace logs aren't too helpful.

Stack & Heap are sufficiently big.

 

Any clues or suggestions?

 

Thanks

 

Update:

- Seems like a watchdog reset from RCM register

- Have tried disabling watchdog  from TCL file, inside __init_registers and __init_hardware. But no success. It still does a WDT reset

标签 (1)
0 项奖励
回复
1 解答
2,165 次查看
Carlos_Musich
NXP Employee
NXP Employee


Hi Kunal,

As your code is running from external RAM I think that without optimizations the code is not fast enough, so watchdog is not being disabled or cleared on time. I recommend to keep optimizations enabled.

Regards,

Carlos

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,166 次查看
Carlos_Musich
NXP Employee
NXP Employee


Hi Kunal,

As your code is running from external RAM I think that without optimizations the code is not fast enough, so watchdog is not being disabled or cleared on time. I recommend to keep optimizations enabled.

Regards,

Carlos

0 项奖励
回复