Is there any JTAG chain reset configuration word for MPC8641D CW8.8.6? I can not erase flash or debug HPCN on my customer board.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any JTAG chain reset configuration word for MPC8641D CW8.8.6? I can not erase flash or debug HPCN on my customer board.

1,340 Views
坤程
Contributor I

I can select the 8641DHPCN_init_core0.cfg for initialization configuration.

174498_174498.png20170116211158.png

Labels (1)
0 Kudos
Reply
1 Reply

1,226 Views
alexander_yakov
NXP Employee
NXP Employee

JTAG file may be used to supply reset configuration word (RCW) only to processor which support this RCW function.

For example MPC83xx family.

For MPC8641D - this processor does not support RCW, all configuration is done by external pins.

Please look MPC8641D Reference Manual, Section 4.4.3 for details.

Because of the above reason, there is no way to override RCW via JTAG, so - no JTAG RCW file for this processor.

If the processor does not work please verify external reset configuration pins, clocking, power supplies and etc.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply