Is there a way to silently install CodeWarrior MCU 10.3?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a way to silently install CodeWarrior MCU 10.3?

2,616 Views
paolobenassi
Contributor I

I need to deploy it to multiple systems in a lab environment. Licensing is being done via FlexLM
.

I used to be able to install 6.3 using the /S /V"/passive" switches, but this will not work anymore.

If someone could point me in the right direction or web link it would be appreciated, I have had no success searching the web or Freescale.

 

Thanks

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

1,976 Views
TICS_Fiona
NXP Employee
NXP Employee

CW10.5 also support silent install (/S /D=c:\Freescale\CW MCU v10.5).

0 Kudos
Reply

1,976 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

we can download CW6.3 special edition from this link:

http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_SPECIALEDITIONS

CW10.3 is no longer available on freescale website. please use CW10.5 from above link if you want to use eclipse version.

does this answer your quesion?

0 Kudos
Reply

1,976 Views
paolobenassi
Contributor I

Sorry, I'm not after the older version of Codewarrior, I only want to know if there are a specific set of command line switches that can be used with setup.exe that will enable a full silent installation of MCU 10.x

thanks

0 Kudos
Reply