Is the P&E USB ColdFire Multilink tool backward compatible with CodeWarrior 10.7 for Microcontrollers? Or do I need to get the P&E USB Universal Multilink tool?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is the P&E USB ColdFire Multilink tool backward compatible with CodeWarrior 10.7 for Microcontrollers? Or do I need to get the P&E USB Universal Multilink tool?

1,238 Views
stephen_krufka
Contributor I

Hello all,

  Is the P&E USB ColdFire Multilink tool (USB-ML-CF Rev C) backward compatible with CodeWarrior 10.7 for Microcontrollers? Or do I need to get the P&E USB Universal Multilink tool to work with CW?  

0 Kudos
Reply
1 Reply

1,182 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Stephen,

Yes, you can use P&E USB ColdFire Multilink tool ( USB ColdFire Multlink|NXP  ) with CW10.7.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply