Is the P&E USB ColdFire Multilink tool backward compatible with CodeWarrior 10.7 for Microcontrollers? Or do I need to get the P&E USB Universal Multilink tool?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is the P&E USB ColdFire Multilink tool backward compatible with CodeWarrior 10.7 for Microcontrollers? Or do I need to get the P&E USB Universal Multilink tool?

1,207件の閲覧回数
stephen_krufka
Contributor I

Hello all,

  Is the P&E USB ColdFire Multilink tool (USB-ML-CF Rev C) backward compatible with CodeWarrior 10.7 for Microcontrollers? Or do I need to get the P&E USB Universal Multilink tool to work with CW?  

0 件の賞賛
返信
1 返信

1,151件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Stephen,

Yes, you can use P&E USB ColdFire Multilink tool ( USB ColdFire Multlink|NXP  ) with CW10.7.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信