Installing codeWarrior in Ubuntu 14.04 LTS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installing codeWarrior in Ubuntu 14.04 LTS

3,630件の閲覧回数
ashwingandhi
Contributor II

can  any one tell the Procedure to install CodeWarrior Development Studio for Power Architecture v10.5.1 - Linux to install in Ubuntu 14.04 LTS.

i tried to follow steps given in readme file to install but its not working..

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,933件の閲覧回数
jinyu_zhang
Fresh Out Contributor

I've installed the version into my Ubuntu 16.04. After you do all the steps in the README file, you need do one more thing. Change directory to the {installed}, and run the install_deps.sh file in the terminal or/and run the detect.sh to verify your completement.

0 件の賞賛
返信

2,933件の閲覧回数
addiyi
NXP Employee
NXP Employee

Your Ubuntu 14.04 is 64bit version? If yes try the steps below:

- follow the steps from Readmee file, Chapter 2.14 Ubuntu 13.10 / 14.04 / 15.04 / Linux Mint 15

- run ./setuplinux script

- run ./runinstall and provide the error/msg

Adrian

0 件の賞賛
返信