Importing CW projects issue from XP to 7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Importing CW projects issue from XP to 7

ソリューションへジャンプ
4,705件の閲覧回数
kylemtg
Contributor II

Hello all,

 

I have some CodeWarrior projects running on windows xp , good . I got a new laptop with W7-64bits, I installed the same version of CW Development Studio 5.9.0.  until here eveything is fine, I am able to create new projects, compile... etc but when I try to open my previous project created under XP, in W7 they are opened as XML files. Weird....

Did someone face the same issue? do you have any clue? Tips?

Thanks a lot in advance

Regards,

Kyle

ラベル(1)
タグ(3)
1 解決策
4,548件の閲覧回数
kylemtg
Contributor II

Hi all,

Ok maybe it's obvious but I hope that could help some beginners like me :smileyhappy: I fixed the problem by exporting the project from an XP machine into an XML format, after that I import it as an XML file in my W7 machine.

Regards,

Khalil

元の投稿で解決策を見る

3 返答(返信)
4,548件の閲覧回数
kylemtg
Contributor II

Here is the correct and practical way to fix this problem:

Go to: edit -> preferences -> General -> IDE Extras and then select ‘Use text-based projects’ option.

4,549件の閲覧回数
kylemtg
Contributor II

Hi all,

Ok maybe it's obvious but I hope that could help some beginners like me :smileyhappy: I fixed the problem by exporting the project from an XP machine into an XML format, after that I import it as an XML file in my W7 machine.

Regards,

Khalil

4,548件の閲覧回数
Monica
Senior Contributor III

Thanks a lot for sharing Khalil! :smileygrin:

Best regards,

Monica

0 件の賞賛
返信