Importing CW projects issue from XP to 7

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Importing CW projects issue from XP to 7

跳至解决方案
4,719 次查看
kylemtg
Contributor II

Hello all,

 

I have some CodeWarrior projects running on windows xp , good . I got a new laptop with W7-64bits, I installed the same version of CW Development Studio 5.9.0.  until here eveything is fine, I am able to create new projects, compile... etc but when I try to open my previous project created under XP, in W7 they are opened as XML files. Weird....

Did someone face the same issue? do you have any clue? Tips?

Thanks a lot in advance

Regards,

Kyle

标签 (1)
标记 (3)
1 解答
4,562 次查看
kylemtg
Contributor II

Hi all,

Ok maybe it's obvious but I hope that could help some beginners like me :smileyhappy: I fixed the problem by exporting the project from an XP machine into an XML format, after that I import it as an XML file in my W7 machine.

Regards,

Khalil

在原帖中查看解决方案

3 回复数
4,562 次查看
kylemtg
Contributor II

Here is the correct and practical way to fix this problem:

Go to: edit -> preferences -> General -> IDE Extras and then select ‘Use text-based projects’ option.

4,563 次查看
kylemtg
Contributor II

Hi all,

Ok maybe it's obvious but I hope that could help some beginners like me :smileyhappy: I fixed the problem by exporting the project from an XP machine into an XML format, after that I import it as an XML file in my W7 machine.

Regards,

Khalil

4,562 次查看
Monica
Senior Contributor III

Thanks a lot for sharing Khalil! :smileygrin:

Best regards,

Monica

0 项奖励
回复