If you know you have codewarrior issues, why not fix them?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

If you know you have codewarrior issues, why not fix them?

909件の閲覧回数
geraldharris
Contributor I

I would like to have a working copy of codewarrior installed to work with a dragon12-light

 

 

MC9S12DG256 processor in less than the 3 weeks I have invested so far.  When I open codewarrior 5.9, I would like to see that processor supported.

 

When I make a phone call to Freescale (that tells me to send an email to ANA@frescale.com) I would like a reply telling me that 64 bit OS are not supported...or any reply at all for that matter.

 

When I buy the small engine kit to learn, I would like the BDM adapter to work on a 64 bit OS, without spending more hours finding out that the included USB to BDM adapter is no longer supported, and that no one has published current drivers for it for years- when I by the dragon board I would like to not have to spend  hours finding out that CW5.1 is required- then spend hours trying to get the licenses and installation incorporated so I can find out that codewarrior 5.1 will basically not work with most windows 64 bit systems, and won't even install.

 

Why?

ラベル(1)
0 件の賞賛
返信
1 返信

843件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Gerald,

About "I can find out that codewarrior 5.1 will basically not work with most windows 64 bit systems", does

the CW5.1 can not installed on your Windows 64 bit PC ?

The CW5.1 support win7 64 bit . You can download it at here : CodeWarrior Dev Tools for HCS12(X) MCUs|NXP

BR

Alice

0 件の賞賛
返信