ICDPPCNEXUS: shows way too many source modules

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ICDPPCNEXUS: shows way too many source modules

1,370 次查看
lucvandeuren
Contributor II

Hello,

 

I am working with ICDPPCNEXUS Debugger(v1.34.00.01) for Codewarrior (IDE 5.9.0)  there are part of Development studio 2.9 for MPC55xx build 111011.

 

When I want to look at the source code before debugging to set breakpoints I use the right click menu "Select Source Module"

 

     It seems strange to me that many files are repeated a 30 times consecutevely!

   

Question: Is there a way to only have one entry in this list pre file?

 

greetings,

 

Luc,

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,256 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hi

CodeWarrior v2.9 is an old version, could you please upgrade to CW2.10? It can be downloaded from:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MPC5XX

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复