I2C write register stuck at i2c_Wait() K60N512

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C write register stuck at i2c_Wait() K60N512

1,406 Views
neagoeiulia
Contributor I

Hello!

 

I try to use the I2C module to configure a CMOS sensor from a Kinetis K60N512  in an application but it gets stuck after the instruction I2C0_D = u8RegisterAddress; at i2c_Wait();.

It worked a  few times, but now it's stopped. Here is my code:

 

void OV7675WriteRegister(unsigned char u8RegisterAddress, unsigned char u8Data)

{

  // send data to slave

  IIC_StartTransmission(SlaveID,MWSR);

  i2c_Wait();

 

 

  I2C0_D = u8RegisterAddress;

 

 

  i2c_Wait(); // here is the problem i don't understand

 

 

  I2C0_D = u8Data;

  i2c_Wait();

 

 

  i2c_Stop();

 

 

  Pause();

}

 

Can anyone tell me what is wrong?

 

Thanks

Iulia

Labels (1)
0 Kudos
Reply
2 Replies

1,156 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi lulia,

Please checked whether  the flag of   I2C0_S -> IICIF  set ?

If no , i think the basic configuration of I2C transmit have some error, please check .

You can refer to some I2C demo code , for example "KINETIS512_V2_SC"

K60_100 |Kinetis K60 100 MHz MCUs|Freescale   ) in the IAR demo , there is a "i2c_demo" .

BR

Alice

0 Kudos
Reply

1,156 Views
albertolubeiro
Contributor III

Hi Alice,

I am using KDS3.0 and KDSK v1.2.0 with PEX and im having the same issue.

In my case, the code get stuck in the following line.

/* Wait for the transfer to finish.*/

    I2C_DRV_MasterWait(instance, timeout_ms);

Inside this function there is the following code:

do

   {

        syncStatus = OSA_SemaWait(&master->irqSync, timeout_ms);

    }while(syncStatus == kStatus_OSA_Idle);

I use the non-blocking function I2C_DRV_MasterSendDat, so it should get out of here because of a time out

Any idea?

I am really concerned. it is pretty urgent issue

Thanks and best regards

0 Kudos
Reply