I2C examples for FRDM KE02Z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C examples for FRDM KE02Z

2,532 Views
yusifnurizade
Contributor III

Hello all,

 

I am trying to talk to a sensor in I2C using the FRDM KE02Z. I am new to both CW and the FRDM so I was wondering if anyone could point me in the direction of some sample code. Sample code for talking to a sensor with I2C is preferred but any I2C examples would be appreciated. The sample code had a I2C portion in lab_demo but as far as I can tell that is not for CW and I was hoping for something specifically dedicated to it like Uart_demo or SPI_demo have.

 

Would appreciate any advice.

 

Thanks,

Yusif Nurizade

 

edit: Issues with lab_demo

Labels (1)
2 Replies

2,132 Views
BlackNight
NXP Employee
NXP Employee

Hello,

I have posted several examples and articles for the FRDM board using I2C (not specific for KE02Z, but with Processor Expert things are the same for all devices):

I2C | MCU on Eclipse

Might be helpful for you, as well the links to GitHub: mcuoneclipse/Examples at master · mcuoneclipse · GitHub

2,132 Views
yusifnurizade
Contributor III

Erich,

Thank you for the link, that's twice this week you have come through for me!

I will be spending quite a bit of time on this site as one of my current projects is closely tied to the FRDM board and I2C. Shooting you an email now for a follow up question.

Thanks again!

Yusif Nurizade

0 Kudos
Reply