I use PE for EEPROM.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I use PE for EEPROM.

2,654 Views
100asong
Contributor I

When I configure IntEEPROM part, a error message occur: ERROR:Compiler option -CpPPAGE=0x15(address of Ppage) or CpPPAGE=RUNTIME must be set to comiler the generated code correctly(current target settings,compiler for HC12,option,Code generation tab,PPAGE register is used for paging......)......

 

How to do it ?

Please let me know.

Thanks.

Labels (1)
0 Kudos
Reply
3 Replies

2,493 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Cang,

to solve this problem, please add  -CpPPAGE=RUNTIME to compiler settings that can fix the problem. see attached screenshot.
can this help you?
2015-03-26_13-56-34.png


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,493 Views
100asong
Contributor I

Please give me EEPROM code for 9S12g128.Thanks.

0 Kudos
Reply

2,493 Views
100asong
Contributor I

Any body help me,thanks.

0 Kudos
Reply