I need to join the S29AL008J55BFIR2 in the configuration file in CW7.2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I need to join the S29AL008J55BFIR2 in the configuration file in CW7.2

823 次查看
xiangli
Contributor I

I need to join the S29AL008J55BFIR2 in the configuration file in CW7.2

标签 (1)
0 项奖励
回复
1 回复

764 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Xiang

The S29AL008J55BFIR2 is not in the list of Flash_Programmer devices that supported:

Freescale\CodeWarrior for ColdFire V7.x\ColdFire_Support\Initialization_Files

Please create it following 6.3 in AN3389:

http://cache.nxp.com/files/soft_dev_tools/doc/app_note/AN3389.pdf

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复