I need CodeWarior 10.6.4 standard edition installation file. I have a license file.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I need CodeWarior 10.6.4 standard edition installation file. I have a license file.

2,646件の閲覧回数
rehan_khan
Contributor III

I need a installation file for CodeWarrior 10.6.4 standard edition. I have a license file for that.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,528件の閲覧回数
schmark
Contributor I

It appears that the Codewarrior V10.6.4 is no longer posted not available; however, I need to support a project that was built with V10.6.4.  How do I obtain the installation for that version?

0 件の賞賛
返信

2,590件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Rehan,

The installation file is the same for the different License.

Please download it at here :

CodeWarrior for Microcontrollers-Eclipse IDE|NXP 

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信