I get messaga L1822. Yet the items are defined

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I get messaga L1822. Yet the items are defined

1,424 次查看
andrewdavis
Contributor I

Yet the items ARE defined.

标签 (1)
0 项奖励
回复
4 回复数

1,230 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Andrew,

In addition, can you check if the objects definition files are included in the build?

in classic CW

pastedImage_1.png

in CW eclipse

pastedImage_2.png

if the problem still can not be solved, can you please upload your project here?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,230 次查看
andrewdavis
Contributor I

Link Error : L1822: Symbol TIMESEQ in file C:\Users\DE\Documents\Project_2\Project_2_Data\Standard\ObjectCode\main.asm.o is undefined

Link Error : L1822: Symbol INITSEQ in file C:\Users\DE\Documents\Project_2\Project_2_Data\Standard\ObjectCode\EXESEQ.asm.o is undefined

Link Error : Link failed

0 项奖励
回复

1,230 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Your zip folder includes some sources files but doesn't include project file (.mcp)

can you please unpload your entire Project_2 project folder in zip. thus we can test and reproduce the problem ?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,230 次查看
BlackNight
NXP Employee
NXP Employee

Hi Andrew,

can you provide any further information?

What microcontroller are you using? S08 or S12?

How have you these ojbects *defined* (declaration is not enough).

You can use the decoder.exe (or the GNU objdump) utility to inspect your files to see exactly what is in it, see https://mcuoneclipse.com/2012/02/05/show-me-your-files-lib/ 

I hope this helps,

Erich

0 项奖励
回复