How to use software interrupt/ timer interrupt on KE06Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use software interrupt/ timer interrupt on KE06Z

2,421件の閲覧回数
eyeow84
Contributor III

I am using FRDM-KE06Z (MKE06Z128VLK4) to control hi and low state on few I/O pins. I am using CW 10.6 Processor Expert (PE) to generate code TimerInt_LDD. I want to set 3 I/O pins to HI during state 1 for 3 minutes, and set/toggle them to LOW during state 2 for 3 minutes. And maintain this loop over a period of time or infinite loop.

 

I am still exploring the options to make this works. I found that one of the possible ways is to use TimerInt_LDD? However I don't have any working example by using this TimerInt_LDD component and the example given in CW help is very insufficient.

 

thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

2,309件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Lee,

I suggest you use component PPG_LDD which has method to change period and duty cycle during program running.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信