How to run initialization script when connect to target through JTAG RCW override

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to run initialization script when connect to target through JTAG RCW override

1,656 次查看
henryeng
Contributor I

Hello

 

I am trying to bring up a new board based on the T1020.  I have connected to the target using code warrior JTAG RCW override.  When I connect to the target this way, code warrior does not give me the option to initialize the cpu (I want to use a modified T1020RDB_core.tcl configured for our target to burn the RCW into NAND flash).  Is there a way to do this?  Note.  The target board is to use the Hard coded RCW (with this method, the initialization option is avail)

 

Thanks

Henry Eng

标签 (1)
0 项奖励
回复
1 回复

1,387 次查看
addiyi
NXP Employee
NXP Employee

After you select the jtag_chain file as Target Type, you can add the init file as in below image:

pastedImage_0.png

Adrian

0 项奖励
回复